Associate II
May 20, 2025 11:11 AM UTC
Solved
STDES-WL5U4SBB: Clarification on FE_CTRL2 and FE_CTRL3 in HighBand HighPower
- 2 replies
- 587 views
I am developing a custom board based on the MB1720 HighBand HighPower reference design using the STM32WLE5CC microcontroller.
I need clarification on the operation and connection of the FE_CTRL2 and FE_CTRL3 signals that control the RF front-end switch (U3 - BGS12SN6):
What is the exact functional role of FE_CTRL2 and FE_CTRL3 in this configuration?
1. From the schematic, FE_CTRL2 is connected to PC13, and FE_CTRL3 to PA11, both controlling the BGS12SN6 SPDT RF switch.
2. How do these signals behave during transmit and receive? Which one is responsible for enabling TX and which one for RX?
3. Additionally, I’ve exposed these FE_CTRL lines to a connector (CN2). Is this standard practice, or should these only be internally controlled by the MCU?