ST67W611M1 target-wake-time function not supported
I am trying to test the target-wake-time (TWT) feature of the ST67 using the CLI firmware. I have attempted to setup a TWT connection on two different routers but both times the ST67 reports “Could not setup TWT” in response to my wifi_twt_setup command. The routers I have tried are the TP-Link AX5400 (Archer AX73) and the EERO Max 7.
Here is an example command sequence:
w61/>Connected to following Access Point :
[8c:dd:0b:e5:ff:c8] Channel: 6 | RSSI: -42 | SSID: EERO
Station got a new IP address : 192.168.4.36w61/>powersave 1
w61/>wifi_twt_setup 1 1 13 128 1000
Could not setup TWT
w61/>wifi_twt_status
TWT not supported
w61/>