Solved
SMPS Clock Mux Errors
- 2 replies
- 1262 views
Whenever I set the SMPS Clock Mux to HSE /4 /2 = 4 I can save the project without errors but whenever I reopen the ioc file I get a warning that there is a clock issue that needs to be fixed. I go into the clock configuration and it's bee reset to HSI /4 /2 = 2 and marked in red as an error. If I click resolve clock issues it changes it to HSI /2 /2 = 4 but I want it to stay at HSE
Other projects I've created for the NUCLEO-WB55 board from the example selector use HSE /4 /2 =4 so I'm wondering if there is a setting that's conflicting. I just can't find it.