Skip to main content
Senior
Sep 12, 2023 5:30 AM UTC
Question

Slow block read with SPI fatfs

Hello,

I measured the performance of uSD card connected through the SPI on Read/Write operation.

The weird thing is that the Block read speed is 3x to 4x slower than the write speed.  I'm writing/read 4kB of data and the SD card is formatted with 4kB allocation unit.

The SPI transaction of the 4k write is about 5-7ms, when considering the SPI transaction of the block read it takes about 20ms.

Does someone have an idea of what the issues can be?

This topic has been closed for replies.

12 replies

ST Technical Moderator
Sep 12, 2023 5:49 AM UTC

Hello @frnt 

Which stm32 product are you using?

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
frntAuthor
Senior
Sep 12, 2023 8:12 AM UTC

Hello @FBL,

STM32WLEx SPI bus is 16MHz

ONadr.1
Senior III
Sep 12, 2023 8:28 AM UTC

I would look directly at the SPI bus with a logic analyzer, where the slowdown occurs.

frntAuthor
Senior
Sep 12, 2023 8:48 AM UTC

Are there some important aspects to be considered in the block read except for the CMD18 command and CMD12 for stopping? I do not have a logic analyzer, I could have a look with the oscilloscope at one block transfer.

ONadr.1
Senior III
Sep 12, 2023 9:00 AM UTC

Try to Saleale USB analyzer. Is cheap and for this work is sufficient.

frntAuthor
Senior
Sep 12, 2023 3:52 PM UTC

Ok, I'll have a look at the Saleae.

Could it be that fatfs does not use DMA for receiving data and using blocking calls?

ONadr.1
Senior III
Sep 12, 2023 6:34 PM UTC
I think reading a 4k block in 20ms is way too slow, even for a blocking function. I suggested using the analyzer to find out how the delay is spread and what could be causing it.
 
frntAuthor
Senior
Sep 22, 2023 8:53 AM UTC

Is the function correct in your opinion?

frntAuthor
Senior
Sep 19, 2023 1:48 PM UTC

@ONadr.1 I'll wait for the purchase. In the meantime, I have tried other micro-SD cards, but same slow speed in block read. 

I'm sharing the block read code, but to me it seems correct:


 

static bool SD_RxDataBlock(BYTE *buff, UINT len)
{
	uint8_t token;
	Timer1 = 200;
	/* loop until receive a response or timeout */
	do {
		token = SPI_RxByte();
	} while((token == 0xFF) && Timer1);

	/* invalid response */
	if(token != 0xFE) return FALSE;

	/* receive */
	do {
		SPI_RxBytePtr(buff++);
	} while(--len);

	/* discard CRC */
	SPI_RxByte();
	SPI_RxByte();
	return TRUE;
}​