Single- / Dual-Core with STM32WLx5: Are both cores connected to SUBGHZ peripherial?
I am confused because I thought I have read somewhere that on the STM32WL55JC, only the M0+ Core is connected to the RF part and therefore M4 core normally hosts app code, M0+ core the RF part.
In the examples I have seen for the Nucleo WL55JC there are mono-core are well as dual-core implementations.
So, is the SUBGHZ just a peripherial just any other and its up to me on which core I use it and furthermore, single-core code written for a STM32WL55 would also work and behave similar on a single-core STM32WLE5?