Skip to main content
Associate III
Aug 20, 2025 9:08 PM UTC
Question

Setting the MTU, the ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE event never fires.

Hello,

I'm trying to figure out why setting the MTU stops the ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE event from ever firing.  This essentially breaks everything.

case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:
	/* USER CODE BEGIN EVT_LE_CONN_COMPLETE */

	hci_le_set_data_length(tpms_handleNotification.ConnectionHandle, /*tx_octets*/251, /*tx_time*/2120);

	tBleStatus result = aci_gatt_exchange_config(tpms_handleNotification.ConnectionHandle);
	if(result != BLE_STATUS_SUCCESS)
	{
		APP_DBG_MSG("\r\n\r** MTU failed to set.\n\r");
	}

	/* USER CODE END EVT_LE_CONN_COMPLETE */
	/**
	 * The connection is done,
	 */
	connection_complete_event = (hci_le_connection_complete_event_rp0 *) meta_evt->data;
	BleApplicationContext.BleApplicationContext_legacy.connectionHandle = connection_complete_event->Connection_Handle;
	BleApplicationContext.Device_Connection_Status = APP_BLE_CONNECTED_CLIENT;

	/* CONNECTION WITH CLIENT */
	APP_DBG_MSG("\r\n\r** CONNECTION COMPLETE EVENT WITH SERVER \n\r");
	handleNotification.P2P_Evt_Opcode = PEER_CONN_HANDLE_EVT;
	handleNotification.ConnectionHandle = BleApplicationContext.BleApplicationContext_legacy.connectionHandle;
	P2PC_APP_Notification(&handleNotification);

	result = aci_gatt_disc_all_primary_services(BleApplicationContext.BleApplicationContext_legacy.connectionHandle);
	if (result == BLE_STATUS_SUCCESS)
	{
	 APP_DBG_MSG("\r\n\r** GATT SERVICES & CHARACTERISTICS DISCOVERY \n\r");
	 APP_DBG_MSG("* GATT : Start Searching Primary Services \r\n\r");
	}
	else
	{
	 APP_DBG_MSG("BLE_CTRL_App_Notification(), All services discovery Failed \r\n\r");
	}
	
break; /* HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE */

Both the server and client have their, CFG_BLE_MAX_ATT_MTU set to 156.  I receive the event and checking the returned value is 156.  All of that seems to be working fine.

case ACI_ATT_EXCHANGE_MTU_RESP_VSEVT_CODE:
{
	aci_att_exchange_mtu_resp_event_rp0 *exchange_mtu_resp = (aci_att_exchange_mtu_resp_event_rp0 *)blecore_evt->data;
	APP_DBG_MSG("**MTU_size = %d \n",exchange_mtu_resp->Server_RX_MTU );
	APP_DBG_MSG("\r\n\r");
	uint16_t Att_Mtu_Exchanged;
	if (exchange_mtu_resp->Server_RX_MTU < CFG_BLE_MAX_ATT_MTU)
	{
		Att_Mtu_Exchanged = exchange_mtu_resp->Server_RX_MTU - 3;
	}
	else
	{
		Att_Mtu_Exchanged = CFG_BLE_MAX_ATT_MTU;
	}
}

break;

If I comment out these lines, I can receive 20 bytes all day long.

hci_le_set_data_length(tpms_handleNotification.ConnectionHandle, /*tx_octets*/251, /*tx_time*/2120);

tBleStatus result = aci_gatt_exchange_config(tpms_handleNotification.ConnectionHandle);
if(result != BLE_STATUS_SUCCESS)
{
	APP_DBG_MSG("\r\n\r** MTU failed to set.\n\r");
}

With those lines in place, the ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE event is never fired.  This seems to be relevant because when that event isn't fired, the connection handle is never set.

aP2PClientContext[index].connHandle= handle;

I'm leaning towards some kind of timing issue because if I set breakpoints and debug, everything magically works, and I can receive more than 20 bytes.

Is there an event I need to catch, should the MTU code be placed somewhere else or am I just thing about/doing this completely wrong?

Any insight would be greatly appreciated.

Kindest regards.

PS. I've reviewed the, BLE_DataThroughput application, now that's an entirely different beast, as well as PM0271.  There was also another document I looked at from another post where the OP was having difficulties with setting the MTU as well.  None of the searches for setting the MTU really had any resolutions.

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Sep 22, 2025 2:02 PM UTC

Hello @kumaichi 

Have you tried to debug your code and check where the issue is Happening exactly.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.