Skip to main content
MWild.4
Associate
Sep 10, 2021 9:32 AM UTC
Question

Send Eddystone beacons without TLM payload doesn't work

I'm working with the Nucleo board with the STM32WB55 with the BLE Stack: stm32wb5x_BLE_Stack_full_fw.bin (V1.12.1) on the Copro. When I'm running the Beacon Example code I can receive the Beacons on the mobile App.

But since I've configured the code once as EddystoneTLM it always sends the Eddystone Beacons (UID/URL) with the TLM payload and I can't remove it.

I've tried to delete it manually in the initialisation (aci_gap_delete_ad_type(AD_TYPE_SERVICE_DATA) before I initialise it with an other Beacon type, but it doesn't make any differences. Even reprograming the Copro hasn't made any differences.

Is that a known bug from the BLE stack, that it doesn't properly clear the TLM flag? Does someone know a workaround?

This topic has been closed for replies.

2 replies

MWild.4
MWild.4Author
Associate
Sep 15, 2021 5:57 AM UTC

Problem solved. The problem was the app that always shows an TLM payload if it receives an Eddystone Beacon from the same address.

EMECH
ST Employee
Sep 20, 2021 7:56 AM UTC

Hello,

Some smartphone applications do not really refresh Beacon information if the UUID address of the Beacon if the same ... A way to force this refresh, is to disable and enable smartphone Bluetooth or delete the stored application data in the smartphone.

Best regards.