Skip to main content
TChan.1
Associate
Nov 1, 2020 11:03 AM UTC
Question

RF pin no output on STM32WB55RGV6.

Hi, recently I made a custom board with STM32WB55RGV6 but my BLE side isn't working.

I used STLink to flash in the CoPro lib FW as shown in the YouTube link below.

https://www.youtube.com/watch?v=AcrbUOhApd0

I used the P2P_Server example for Nucleo board and verified the same code works on the Nucleo board.

I used a 3GHz spectrum analyser to check on the RF pin output via direct connection but I saw nothing emitted across the whole band.

I tried to read the version with STM32Programmer but all wireless FW FUS version read options are grey and no way to check on the BLE FW version loaded inside.

So, I am wondering if there is anyway that I can check the loaded FW version, i.e. "stm32wb5x_BLE_Stack_full_fw" the M0 core? Even though it showed "Loaded successfully", is there anyway to double check?

Thanks in advance.

This topic has been closed for replies.

2 replies

Taxara
Associate III
Nov 4, 2020 3:00 PM UTC

Hi,

It should be possible, https://www.st.com/resource/en/application_note/dm00513965-st-firmware-upgrade-services-for-stm32wb-series-stmicroelectronics.pdf mentioned this a few times. See chapter FAQ.

In addition Remi QUINTIN (ST Employee) posted a bat script a while ago in https://community.st.com/s/question/0D50X0000Boyp5q/stm32wb55ceux-custom-board-ble-stack-updating . Perhaps it is of use for you. It is capable of updating your firmware as well as showing the FUS version.

Good luck!

Taxara
Associate III
Nov 6, 2020 10:58 AM UTC

If you want to check it from software you might use this piece of code:

WirelessFwInfo_t WirelessInfo;
 
 /* Read the firmware version of both the wireless firmware and the FUS */
 SHCI_GetWirelessFwInfo( &WirelessInfo );
 
 APP_DBG_MSG("Wireless Firmware version %d.%d.%d\n", WirelessInfo.VersionMajor, WirelessInfo.VersionMinor, WirelessInfo.VersionSub);
 APP_DBG_MSG("Wireless Firmware build %d\n", WirelessInfo.VersionReleaseType);
 APP_DBG_MSG("FUS version %d.%d.%d\n\n", WirelessInfo.FusVersionMinor, WirelessInfo.FusVersionMinor, WirelessInfo.FusVersionSub);