Skip to main content
Visitor
Sep 11, 2026 8:28 AM UTC
Solved

Request for ZOPT (Load-pull) data for STM32WLE5CCU6 at 475 MHz

Hi ST Community,

I am designing a custom board with STM32WLE5CCU6 (UFQFPN48 package) for a LoRa application in the 470–510 MHz band.

I will use RFO_LP only, with +14 dBm output power and VDD_MCU = 3.3 V.

Could you please provide the ZOPT (optimal impedance) for the PA output matching network at 475 MHz for this configuration?

AN5457 Appendix A only covers 868/900/915/923 MHz, so I cannot find the data for 475 MHz. If there is any reference design or application note for this frequency, please point me to it.

Thank you very much.

Imen.DBest answer
ST Technical Moderator
Sep 30, 2026 8:46 AM UTC

Hello ​@InkWn and welcome to the Community,

We do not have the ZOPT at 475 MHz, but we can share the optimal impedance at 490 MHz:

490MHz : Zopt = 7.8 + j*27.2

I recommend you these RF guidelines which may help you on your project:

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Sep 30, 2026 8:46 AM UTC

Hello ​@InkWn and welcome to the Community,

We do not have the ZOPT at 475 MHz, but we can share the optimal impedance at 490 MHz:

490MHz : Zopt = 7.8 + j*27.2

I recommend you these RF guidelines which may help you on your project:

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks