Question
Receiving unexpected LoRaWAN MAC commands on OnRxData (Application layer)
Hi everyone!
I'm working with STM32WLE5CC chips and developing the firmware using STM32Cube FW_WL V1.2.0.
In general the motes are working fine in Lorawan Class C mode.
The issue I'm observing is that in a random way (once or twice in a day) the motes receive a downlink frame which is not sent by the high level application behind NS (ChirpStack).
As you can see in the mote's logs the mote detects it with a FCnt=0 (it should be much higher) and FPort=0. Based on the FPort=0 it should be a MAC command so it shouldn't be passed to the mote application layer handled by the OnRxData callback in the firmware.
2023-07-26 00:32:17,236 - usb1 - INFO - 136193s478:MAC rxDone
2023-07-26 00:32:17,244 - usb1 - INFO - ###### D/L FRAME:0000 | PORT:0 | DR:8 | SLOT:C | RSSI:-105 | SNR:-24
2023-07-26 00:32:17,248 - usb1 - INFO - 136193s484:RX_C on freq 923300000 Hz at DR 8
2023-07-26 00:32:17,255 - usb1 - INFO - 136193s485: >>>>>> DOWNLINK received: 518350011080de2f8eac55d055acae1f9388273b. << this log is generated in the OnRxData function by my code
2023-07-26 00:32:17,260 - usb1 - INFO - 136193s485: >>>>>> Unknown command received. << this log is generated in the OnRxData function by my code
2023-07-26 00:32:49,739 - usb1 - INFO - 136225s984:MAC rxTimeOut
2023-07-26 00:32:49,742 - usb1 - INFO - 136225s984:HDR KO
After receiving this frame sometimes the motes get stuck and hung, and stop responding to downlink commands and stop sending uplink frames as well.
At first I thought it could be an interference causing the mote to interpret it as a DL, but after reviewing the Lorawan modules and specifications I think that is almost impossible.
The other thing that made me think about an interference is that the RSSI for these frames (-105) is much lower than an expected frame (-40, I'm very close to my GW).
Have you experimented with something similar?
Could be it a multicast frame coming from another GW?
The other thing I'll try is the v1.3.0 of the ST library, maybe I'm hitting a bug?
Thanks!