Skip to main content
Associate
Dec 9, 2025 8:25 AM UTC
Solved

Re: How to solve "Error: No STM32 target found!" using Nucleo-WB0?

I have NUCLEO-WB05K/NUCLEO-WB07CC/NUCLEO-WB09KE only the NUCLEO-WB09KE can be connected to with Software Reset mode.

The NUCLEO-WB05K/NUCLEO-WB07CC boards have the above error on connect.

The Hardware Reset mode doesn't work with the NUCLEO-WB09KE (or the other boards).

All STLink firmware up to date - not many jumper options to get wrong on these boards. 

Windows 11.

Imen.DBest answer
ST Technical Moderator
Dec 9, 2025 8:42 AM UTC

Hello @mpj1 

You might have encountered the issue described in this article: 

Establishing the initial connection with NUCLEO-WB05KZ, 7CC, and 9KE boards

So, try entering bootloader mode using the correct jumper settings to recover the boards.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Dec 9, 2025 8:42 AM UTC

Hello @mpj1 

You might have encountered the issue described in this article: 

Establishing the initial connection with NUCLEO-WB05KZ, 7CC, and 9KE boards

So, try entering bootloader mode using the correct jumper settings to recover the boards.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
mpj1Author
Associate
Dec 9, 2025 9:02 AM UTC

Setting the JP1 to BOOTLoader and and connection mode to Normal/Hot plug I've manage to connect by holding the reset button and connecting as soon as I can when releasing the reset button.....