Queue usage fault
Hi
I use free-rtos with stm32wb55.
I use some queues, they all behave as expected except for one of them (led driver queue).
It seemed that some of the messages being sent (to the led driver queue) are ignored or missed.
I added a debug code and found out that the number of messages being sent to the queue is equal to the messages being received but the content being sent is sometime different. I explored it and found out that messages being sent shortly one after another are being "recieved" the same as the last: for example: if 3 messages being sent (with no delay between them) it is received as 3 same messages which are equal to the last message (from the 3 messages).
A delay between mesaages sending sometimes help.
What can be the problem ?
Thanks