Skip to main content
Senior III
Nov 26, 2025 2:55 PM UTC
Solved

Question about WB55 Nucleo ADC example

I'm trying to implement the ADC to get V_BAT. I've done the set up in CubeMX in the IDE.

I then went to the examples to see how a single ADC reading was done. I'm confused about the use of the following variables...

 

/* Variables for ADC conversion data */
__IO uint16_t uhADCxConvertedData = VAR_CONVERTED_DATA_INIT_VALUE; /* ADC group regular conversion data */

/* Variables for ADC conversion data computation to physical values */
uint16_t uhADCxConvertedData_Voltage_mVolt = 0; /* Value of voltage calculated from ADC conversion data (unit: mV) */

/* Variable to report status of ADC group regular unitary conversion */
/* 0: ADC group regular unitary conversion is not completed */
/* 1: ADC group regular unitary conversion is completed */
/* 2: ADC group regular unitary conversion has not been started yet */
/* (initial state) */
__IO uint8_t ubAdcGrpRegularUnitaryConvStatus = 2; /* Variable set into ADC interruption callback */

 

In the rest of the example code these are used as if they were reading & writing directly from & to the ADC registers,

 

 while (1)
 {
 /* Reset status variable of ADC group regular unitary conversion before */
 /* performing a new ADC group regular conversion start. */
 ubAdcGrpRegularUnitaryConvStatus = 0;
 
 /* Init variable containing ADC conversion data */
 uhADCxConvertedData = VAR_CONVERTED_DATA_INIT_VALUE;
 
 /*## Start ADC conversions ###############################################*/
 
 /* Start ADC group regular conversion with IT */
 if (HAL_ADC_Start_IT(&hadc1) != HAL_OK)
 {
 /* ADC conversion start error */
 Error_Handler();
 }
 
 /* Wait till conversion is done */
 while (ubAdcGrpRegularUnitaryConvStatus == 0);

 /* Note: ADC conversions data are stored into variable */
 /* "uhADCxConvertedData". */
 }

 

Yet I cant find anywhere in the code where these links are made. Can someone explain to me what's going on here?

 

 

1 reply

TDK
TDKBest answer
Nov 26, 2025 3:01 PM UTC