Skip to main content
Associate
Sep 16, 2025 4:35 PM UTC
Solved

Programming NUCLEOWB55RG board with another board

I want to program a NUCLEOWB55RG board with another identical NUCLEOWB55RG. 

The reason is the other NUCLEO board is placed on a PCB and is powered externally, so i cannot connect USB to it. 

Do I just remove the JP1 jumper and connect the SWD pins (SWD, SWDIO, GND, VDD, NRST) between boards? 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 16, 2025 5:25 PM UTC

Hello @fshaikh98 

I advice you to use the JP5 of both boards for connections. You may also refer to this article with this article too.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

TDK
Sep 16, 2025 4:56 PM UTC

Why is connecting USB a problem? If external power is connected, it'll use that instead of USB if you have the jumpers configured appropriately.

TDK_0-1758041576168.png

 

But yes, if you connect SWDIO/SWCLK/GND/SWD at the JP5 header, it should work. JP1 is a power header, doesn't seem relevant here.

"If you feel a post has answered your question, please click ""Accept as Solution""."
fshaikh98Author
Associate
Sep 16, 2025 4:58 PM UTC

@TDK External power is 3.3V here, not 5V. I am afraid of the regulator's output affecting the 3.3V input 

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 16, 2025 5:25 PM UTC

Hello @fshaikh98 

I advice you to use the JP5 of both boards for connections. You may also refer to this article with this article too.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.