Skip to main content
RCool.1
Associate
Apr 18, 2023 1:01 AM UTC
Solved

Programming a Nucleo-WBA52CG

I was able to program two Nucleo-WBA52CG using STM32CubeIDE and the on board ST-Link. I programmed them with the BLE_HeartRateThreadX example application. When I power them I can see the BLE_HeartRateThreadX BLE traffic on my phone. However, I can not reprogram them again using the same setup. I suspect the problem is simple but I really have no idea what is wrong. Any help is appreciated. I get the error below when I try to program them.

 

------ Switching to STM32CubeProgrammer -----

[36m[01m     -------------------------------------------------------------------

[39;49m[36m[01m                       STM32CubeProgrammer v2.13.0                 

[39;49m[36m[01m     -------------------------------------------------------------------

 

[39;49m[39;49m

 

[39;49m[39;49mLog output file:  /tmp/STM32CubeProgrammer_dw6pY8.log

[39;49m[00;31mError: Unable to connect to the target device, Access port is not valid.

[39;49mEncountered Error when opening /home/blue/.eclipse/com.st.stm32cube.ide.mcu.rcp.product_1.10.1_139059409_linux_gtk_x86_64/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_2.0.600.202301161003/tools/bin/STM32_Programmer_CLI

 ------ Switching context -----

Error in STM32CubeProgrammer

GDB session terminated: Client connection lost

GdbSessionManager, session terminated: 1

GDB session terminated: Client connection lost

GdbSessionManager, session terminated: 2

GdbSrv, last session terminated, signal dispose

Stopping port 61234

Received stop for port 61234, not accepting new connections.

GdbSrv, deInit entry.

Shutting down...

GdbSessionManager, deInit entry.

GDB session disposed: 2

GDB session disposed: 1

GdbSessionManager, deInit exit

SwvSrv deInit entry

Stopping port 61235

Received stop for port 61235, not accepting new connections.

SwvSrv deInit exit

Stm32Device, closeDevice() entry

Stm32Device, closeDevice() exit

Stm32Device, deInit success

GdbSrv, deInit exit.

Exit.

This topic has been closed for replies.
RCool.1
RCool.1Best answer
Associate
Apr 30, 2023 7:06 PM UTC

Using the stand alone STM32CubeProgrammer I was able to erase the entire flash and get control of the device

1 reply

RCool.1
RCool.1AuthorBest answer
Associate
Apr 30, 2023 7:06 PM UTC

Using the stand alone STM32CubeProgrammer I was able to erase the entire flash and get control of the device