Skip to main content
E.C.
Associate II
Jul 11, 2022 3:20 PM UTC
Question

Problems with ZigBee custom cluster

Greetings,

Recently I tried to implement a ZigBee custom cluster by taking inspiration from the custom long string cluster.

Basically, the client is requesting data by using ZbZclClusterCommandReq and the server is answering thanks to the ZbZclClusterCommandRsp.

I noticed that when the server is the coordinator nothing goes wrong, but if it is a router, the registered client callback returns a status ZCL_STATUS_TIMEOUT.

In order to analyze the problem, I replaced the ZbZclClusterCommandRsp function with ZbZclClusterCommandRspWithCb in order to get the status after the message was enqueued. The status I received in the callback was ZB_APS_STATUS_INVALID_PARAMETER.

What can be the cause of this error? Is there a way to get more details about this error?

Thanks in advance,

E. C.

This topic has been closed for replies.