Skip to main content
Associate III
Jan 30, 2025 10:19 AM UTC
Question

Problems with USART2 Rx Callback with BLE_p2pServer_ota example

Hi,

i am using the BLE_p2pServer_ota example with NUCLEOWBA55 and i want transmitt a 20 Byte package over USART2 with DMA in circular mode (19200 Baud). Here as an example, i send 20 bytes every second via HTerm to USART2. BLE advertising (every 2s) is working (but i am not connected to the cellphone app). 

The Rx Callback function is inside p2p_server_app.c and here i want to toggle the blue LED:

/* USER CODE BEGIN FD_LOCAL_FUNCTIONS*/
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
 if(huart->Instance == USART2)	// Rx Callback for USART2
 {
	BSP_LED_Toggle(LED_BLUE);
 }
/* USER CODE END FD_LOCAL_FUNCTIONS*/

But after several transmissions (between 50 and 150) the callback function is no longer called.

Does anyone have an idea what is going wrong?

This topic has been closed for replies.

23 replies

STTwo-32
ST Technical Moderator
Jan 30, 2025 10:26 AM UTC

Hello @ledi7 

This is not a normal behavior. Could you please try to reproduce it on a simple Code (not inside the Example).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ledi7Author
Associate III
Jan 30, 2025 12:34 PM UTC

I have created a new project from scratch and i am using USART2 with GPDMA in non-circular and circular mode. Also using 20 byte packets with 19200 baud and everything works fine.

 

STTwo-32
ST Technical Moderator
Jan 30, 2025 12:58 PM UTC

So, try to check in case the problem appears if the reception is really ended or not.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Jan 30, 2025 1:56 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ledi7Author
Associate III
Jan 30, 2025 2:00 PM UTC

 Yes, but now only under the account ledi7

ledi001
Associate III
Jan 19, 2025 8:37 AM UTC

Duplicate - merged.


Hi,

I use the example “BLE_p2pServer_ota” with NUCLEO-WBA55 as a template for a project. Once a BLE connection is established with the mobile app, I start sending 20 bytes every 3 seconds via a hyperterminal on USART2 and transmitting it as a notification. The transmission basically works, but after a few transmissions (usually between 5 and 15 transmissions) the HAL_UART_RxCpltCallback function is no longer called. I have tried DMA in normal mode and in circular mode. In circular mode it works a bit longer.

1. in main.c i start the UART2 in DMA receive mode:

 

 

 /*##-2- Put UART peripheral in reception process ###########################*/
 /* Any data received will be stored in "aRxBuffer" buffer : the number max of
 data received is 20 */
 if (HAL_UART_Receive_DMA(&huart2, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK)
 {
 //Transfer error in reception process
 Error_Handler();
 }

 

 

2. in Rx callback function i call the task to send a notification. (This is the same task which is used for button1 in the example)

 

 

/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
 if(huart->Instance == USART2) // Rx Callback for USART2 as soon as 20 bytes received
 {
	 UTIL_SEQ_SetTask( 1<<CFG_TASK_SEND_NOTIF_ID, CFG_SEQ_PRIO_0);
 }
}
/* USER CODE END 4 */

 

 

The task was called a few times but never longer as 15 times. 

How can i solve this problem?