Problems with CAN comunication to STM32WL using MCP2515
Hy, I'm currently working on a project that requires CAN and that information needs to be sent via wireless, for that reason, I chose the NUCLEO stm32WL board. To make the CAN work I have to use the MCP2515 module, that converts CAN to SPI so that the uC can read it. The problem I'm facing is that there's not much content about this board and much less about the matter. The only library I found is this one: https://github.com/eziya/STM32_SPI_MCP2515).
For the project, I need mainly to receive CAN data from another circuit board, and the baudrate of the bus is 500Kbps, which I set on the SPI configuration. However, I'm having troubles receiving such messages, since I can't read any data that is sent. I'm currently using that library, and altered the "stm32f1xx_hal." library for the "stm32wlxx_hal.h" one and with that it should be working. I could use some help to know if I'm configuring something wrong, or if I need to make some changes on the library, or if there's something about the board that needs to be done that I don't know about.
Appreciate the answers!!