Problems with ATSlave connecting to the TTN Network.
Hey there
We are developing LoRa Applications based on I-CUBE-LRWAN Stack. 1.5 Years ago, i ported it into a freertos and it worked great. now i'm trying to port the newer version of the stack and i'm not able to connect to the things network. to my own gateway it isn't a problem at all and the nodes with the old firmware can connect to ttn without a problem. Now i'm running the ATSlave Example on the B-L072z-LRWAN Evaluation kit and i'm not able to connect to TheThingsNetwork either. Does anybody has the same issues? It's really strange because it worked with the old stack and now i'm confused and stuck...