Skip to main content
LBasi.1
Visitor II
Jun 17, 2020 5:16 PM UTC
Question

Problem with USART1 on board B-L072Z-LRWAN1

Hello, everyone.

I have a problem with the board B-L072Z-LRWAN1. 

I edited the End_Node project of I-CUBE-LRWAN in order to get some packets transmitted by a Decawave device connected to the B-L072-LRWAN1 board.

Obviously, I connected the TX-RX pins of my Decawave device to the RX-TX pins of my board (USART1 PA10 - PA9).

Such packets, once received and processed by the board, will be forwared to a Lora gateway for further processing.

The communication between the end node and Lora gateway doesn't seem to give any problems; however, I don't get any packet transmitted by the Decawave device on my B-L072-LRWAN1 if I use USART1.

I don't know why, but I believe that there are some problems with USART1 and the interrupt service routine.

For debugging purposes, I also checked that the Decawave packets are correctly sent and printed to the USART2 (connecting the TX pin of my Decawave to the RX pin of USART2 - PA3) of the B-L072-LRWAN1 board. I confirm there are no problems in this sense, my Decawave packets are correctly sent and printed to the console.

As proof of concept, I also implemented a basic interrupt function that transmits over USART2 the same character read in Tera Term and it worked.

If I try to edit the UART/GPIO parameters of the USART2 in order to receive Decawave packets on the RX pin of the USART1, nothing seems to work (except the communication with the Lora gateway).

I initialized the USART1 and interrupt service routine in the following way:

...
 
UART_HandleTypeDef 	huartHandle1;
 
void USART1_IRQHandler(void)
{
  HAL_UART_IRQHandler(&huartHandle1);
}
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{ 
 if (huart->Instance == USART1)
 {
 HAL_UART_Receive_IT(&huartHandle1, buff, 32);
 ...
 }
}
  
void gpioInit()
{
	GPIO_InitTypeDef GPIO_InitStruct;
	__GPIOA_CLK_ENABLE();
	GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
	GPIO_InitStruct.Alternate = GPIO_AF4_USART1;
	HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
 
void huartHandleInit()
{
 __USART1_CLK_ENABLE();
	huartHandle1.Instance = USART1;
	huartHandle1.Init.BaudRate = 115200;
	huartHandle1.Init.WordLength = UART_WORDLENGTH_8B;
	huartHandle1.Init.StopBits = UART_STOPBITS_1;
	huartHandle1.Init.Parity = UART_PARITY_NONE;
	huartHandle1.Init.Mode = UART_MODE_TX_RX;
	huartHandle1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
	huartHandle1.Init.OverSampling = UART_OVERSAMPLING_16;
	HAL_UART_Init(&huartHandle1);
  HAL_NVIC_SetPriority(USART1_IRQn, 0, 0);
	HAL_NVIC_EnableIRQ(USART1_IRQn);
}
...
 
main()
{
 /* STM32 HAL library initialization*/
 HAL_Init();
 
 /* Configure the system clock*/
 SystemClock_Config();
 
 /* Configure the debug mode*/
 DBG_Init();
 
 /* Configure the hardware*/
 HW_Init();
 
 gpioInit();
 
 huartHandleInit();
 
 HAL_UART_Receive_IT(&huartHandle1, buff, 32);
 
 while (1)
 {
 ...
 }
}

What could be the problem of using the USART1 on board B-L072Z-LRWAN1?

Thanks in advance.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
Jun 18, 2020 6:31 AM UTC

Maybe the reason is the pins PA9 and PA10 and therefore USART1 are fixed connected with the Murata LoRa module.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.