Problem with sending message longer than 4 characters & Problem with firmware update
Hi,
I've got 2 I-Nucleo-LRWAN1 shields on 2 STM32 Nucleo64 F103-RB boards. I've uploaded PingPong example from : https://github.com/stm32duino/I-NUCLEO-LRWAN1 and it works but when I've tried to modify code and send longer message (for example "ABCDEFG123") i received on second board only first four characters "ABCD".
I checked modules by BridgeSerial and it works. Software version is: 2.9.
I cannot update firmware to newer version, after connection to ST-Link on STM32 Board there is info in ST-Link utility that it has Read Out Protection.
I also paste my simple code I used for testing.
Tx:
#include "LoRaRadio.h"
#define SEND_PERIOD_MS 2000
HardwareSerial SerialLora(PC_11, PC_10);
uint8_t Message[] = "ABCDEFGH";
//uint8_t len=0;
//int timer=0;
//uint8_t x=0;
void setup() {
Serial.begin(115200);
Serial.println("!! Tx !!");
while(!loraRadio.begin(&SerialLora)) {
Serial.println("LoRa module not ready");
delay(1000);
}
Serial.println("LoRa module ready\n");
}
// len=sizeof(Message);
// loraRadio.write(Message,len);
// timer=millis();
//
void loop() {
//len=sizeof(Message);
loraRadio.write(Message,9);
Serial.println("Message sent : ");
//Serial.println(x);
delay(3000);
}Rx:
#include "LoRaRadio.h"
HardwareSerial SerialLora(PC_11, PC_10);
//uint8_t x=0;
void setup() {
// put your setup code here, to run once:
Serial.begin(115200);
Serial.println("!! Rx !!");
while(!loraRadio.begin(&SerialLora)) {
Serial.println("LoRa module not ready");
delay(1000);
}
Serial.println("LoRa module ready\n");
}
// if(loraRadio.read(rcvData) > 0) {
// Serial.println((char *) rcvData);
// }
//}
void loop() {
uint8_t rcvData[64];
// put your main code here, to run repeatedly:
if(loraRadio.read(rcvData) > 0){
Serial.println("Receiver");
Serial.println((char *)rcvData);
delay(500);
Serial.println((char *)rcvData);
}
//Serial.println((char *)rcvData);
// if(x > 0) {
//Serial.println((char *) rcvData);
// Serial.println(x);
memset(rcvData, 0, 10);
delay(1000);
}I'd be grateful for any help.
Thanks in advance!
T.