Skip to main content
Associate III
March 24, 2025
Solved

Problem with entering standby mode in STM32WB55 when BLE is already initialized

Hello
I'm trying to make an application with BLE using this video tutorial https://www.youtube.com/watch?v=CKYWy7LKL68&ab_channel=STMicroelectronics.

I also found an example of entering standby mode using RTC wake-up (PWR_STANDBY_RTC in the example projects). I rewrote the program so that wake-up works on alarm. The program seems to work fine, but only if I enter standby mode before BLE initialization in CPU2 using MX_APPE_Init();.

As far as I understand, I have to turn off BLE and de-initialize RF the stack? How do I stop the second core from running?

I found this function in my BLE code: Adv_Cancel(); but it doesn't help.

Here is the main part of my code:

int main(void)
{

 HAL_Init();
 MX_APPE_Config();
 SystemClock_Config();
 PeriphCommonClock_Config();
 MX_IPCC_Init();
 MX_RF_Init();//sets alarm for 5 sec
 MX_GPIO_Init();
 MX_SPI1_Init();
 MX_ADC1_Init();
 MX_I2C3_Init();
 MX_TIM17_Init();
 MX_TIM16_Init();
 MX_RTC_Init();

 if( (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
 && (__HAL_PWR_GET_FLAG(PWR_FLAG_C2SB) != RESET)
 )
 {
	 HAL_GPIO_TogglePin(LED2_GPIO_Port, LED2_Pin);
	 HAL_Delay(1000); // Мигаем светодиодом 1 секунду

 // Clear Standby flag
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_C2SB);
 }


 MX_APPE_Init();

	Adv_Cancel();
	EnterStandBy();

 while (1)
 {

 /* USER CODE END WHILE */
 //MX_APPE_Process();
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

void EnterStandBy(void)
{
	 HAL_NVIC_SetPriority(RTC_Alarm_IRQn, 0, 0);
	 HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);

	 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
	 HAL_NVIC_DisableIRQ(RTC_WKUP_IRQn);

	 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

	 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
	 __HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF);

	 if ((LL_PWR_IsActiveFlag_C1SB() == 0) || (LL_PWR_IsActiveFlag_C2SB() == 0))
	 {
	 LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);
	 }

	 HAL_PWR_EnterSTANDBYMode();
}

Let me know if more information is needed.

I also found this example https://github.com/stm32-hotspot/STM32WB-BLE-standby/tree/main but I can't find anything in it related to turning off the second core. 

I also tried removing the commands that were commented out as specific to cpu1 when cpu2 was not initialized.

I also saw some messages about resetting the HCI but my board freezes when I do it.

In some developer chats, there are legends about problems with sleep for the second core, which the developer of Flipper Zero had. Also, from some comments in his code, it becomes clear that this was a sore subject for them.
Help, please. I will be immensely grateful for your help.

 

FilipKremen
FilipKremenBest answer
ST Employee
April 3, 2025

Hello,

interrupt for alarm needs to be enabled. You can check the configuration in HAL_RTC_MspInit() function. (stm32wbxx_hal_msp.c file)

I'm attaching the project also with alarm wake up possibility.

I hope it will work on your side.

 

Best regards,

ST support

9 replies

FilipKremen
ST Employee
March 25, 2025

Hello,

the wireless stack manages CPU2 low power mode on its own. Please have a look here.

How to build wireless applications with STM32WB MCUs - Application note section 4.6

I'm also attaching modified STM32WB-BLE-Standby example. The MCU can be woken up by grounding PC5 pin or automatically in 10 s using RTC wakeup. You should be able to measure around 2 uA (IDLE) with STM32WB55 Nucleo board removing JP2. Also please remove all from JP5 and disconnect USB cable from ST-Link.

 

Best regards,

Filip Kremen

IlliaGxAuthor
Associate III
March 25, 2025

Can I use some kind of this function to put the device to sleep by pressing a button?

void Disconnect_BLE_And_Enter_Standby(void)
{
 
 if (BleApplicationContext.Device_Connection_Status != APP_BLE_IDLE)
 {
 aci_gap_terminate(BleApplicationContext.BleApplicationContext_legacy.connectionHandle, 0x13);
 }

 
 if (BleApplicationContext.Device_Connection_Status == APP_BLE_FAST_ADV ||
 BleApplicationContext.Device_Connection_Status == APP_BLE_LP_ADV)
 {
 aci_gap_set_non_discoverable();
 }

 
 Go_standby();
}

 

FilipKremen
ST Employee
March 27, 2025

Hello,

you can enter standby mode by pressing the button with this code below (in this case it's SW3).

void APP_BLE_Key_Button3_Action(void)
{

	 if (BleApplicationContext.Device_Connection_Status != APP_BLE_IDLE)
	 {
	 aci_gap_terminate(BleApplicationContext.BleApplicationContext_legacy.connectionHandle, 0x13);
	 }

	 aci_hal_stack_reset();

	Go_standby();

}

Best regards,

Filip Kremen 

IlliaGxAuthor
Associate III
March 29, 2025

Hello,

thank you very much for your support!
Unfortunately, I get into HardFault_Handler when executing aci_hal_stack_reset();.
I also did not find a call to such a function in the example that you gave.
Perhaps there are some pitfalls in this application, some hidden settings that I can miss in my project? I compared the code of the p2p server and your project, and there are not many differences at first glance.
Sorry for the hassle, but it is very difficult to analyze these projects. I work with a custom board, but I made a simple example on the WB55 Nucleo board based on this video https://www.youtube.com/watch?v=CKYWy7LKL68, which anyone can run. It automatically turns on the alarm for 5 seconds. I made some changes in the files app_entry.c, app_ble.c, app_conf.h and marked them with the comment // added

I apologize for the impudence, but could you take a look at this? I think the solution to this problem will be useful to the entire WB community, and this thread can be helpful to many people.

FilipKremen
ST Employee
April 1, 2025

Hello,

I checked your project, and I noticed you commented MX_APPE_Process() line.

This function is running the sequencer which you can imagine like a while loop for task scheduling.

It's recommended to use it because it avoids race condition when LP modes are implemented.

If you want to read data from sensors or sending data via ACI commands, you should register the tasks first before running them in the sequencer.

Please visit website below for more information.

Utility:Sequencer - stm32mcu

I'm also attaching the modified standby example. Please have a look at README file for more information and let me know if it works on your side.

 

Best regards,

ST support

IlliaGxAuthor
Associate III
April 1, 2025

Hello
Thank you very much for your help. Your project is working properly. I was also able to transfer the functionality to my application. I think this project deserves to be in the ST GitHub more than the original example I referenced earlier.
I hate to bother you with questions after such great help you have provided, but now I am having a problem with RTC Alarm.
I tried replacing a working RTC wake-up timer with an RTC Alarm, but it doesn't work (the board goes to sleep, and that's it). Can you please tell me how to fix the problem?
If necessary, I can close this thread by marking your answer as correct and make a new thread about RTC Alarm, where you can reply. Let me know the best way to handle it.
Regards

FilipKremen
FilipKremenBest answer
ST Employee
April 3, 2025

Hello,

interrupt for alarm needs to be enabled. You can check the configuration in HAL_RTC_MspInit() function. (stm32wbxx_hal_msp.c file)

I'm attaching the project also with alarm wake up possibility.

I hope it will work on your side.

 

Best regards,

ST support

IlliaGxAuthor
Associate III
April 3, 2025

Hello
Just in case for the future, when I try to compile your project, I get the error 

make: *** No rule to make target 'C:/Users/kremenfi/OneDrive - STMicroelectronics/PROJECTS/Examples/STM32WB/P2P_Server_Standby/Utilities/lpm/tiny_lpm/stm32_lpm.c', needed by 'Utilities/stm32_lpm.o'. Stop.

But I transferred your functions to my project, and now RTC Alarm works!
I cannot thank you enough! Your assistance was a lifesaver.

I wish you good luck in life!
Best regards