Problem with DMA interrupts and low power sleep mode
Hello everyone, I am trying to code a program that uses DMA to transfer samples from an external codec through the SAI.
The CPU is in Low Power sleep for most of the time between the DMA interrupts
After each DMA interrupt whether its half-complete or complete, the CPU exists low power sleeps and executes a function on the samples from that the DMA fetched, then it goes to sleep.
Unfortunately, the CPU exists low power sleep too fast, and apparently it's not the DMA that wakes it up. in fact, I cant even see anything in the interrupt log that might solve this "phantom interrupt" mystery.
These are the main parts of the code
Main while loop:
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_SuspendTick();
SystemClock_Decrease();
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, 1);
HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON,
PWR_SLEEPENTRY_WFI);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, 0);
HAL_PWREx_DisableLowPowerRunMode();
SystemClock_Config();
HAL_ResumeTick();
// Add algorithm code here
//
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
Clock config:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSI
|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 32;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV8;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
|RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
/** Initializes the peripherals clocks
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_SAI1
|RCC_PERIPHCLK_I2C1|RCC_PERIPHCLK_USB;
PeriphClkInitStruct.PLLSAI1.PLLN = 24;
PeriphClkInitStruct.PLLSAI1.PLLP = RCC_PLLP_DIV2;
PeriphClkInitStruct.PLLSAI1.PLLQ = RCC_PLLQ_DIV2;
PeriphClkInitStruct.PLLSAI1.PLLR = RCC_PLLR_DIV2;
PeriphClkInitStruct.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_SAI1CLK;
PeriphClkInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;
PeriphClkInitStruct.Sai1ClockSelection = RCC_SAI1CLKSOURCE_PLLSAI1;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSI;
PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}Clock decrease
void SystemClock_Decrease(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
/* Select MSI as system clock source */
/* Note: Keep AHB and APB prescaler settings from previous structure initialization */
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/* Disable PLL to reduce power consumption since MSI is used from that point */
/* Change MSI frequency */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_OFF;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
What might be causing the problem?