Skip to main content
Associate III
May 13, 2025 1:59 PM UTC
Solved

Problem with ADC on custom board

Hello.
I have a problem with the ADC on the custom board with the STM32WB55 chip. I am using a divider and should get something around 2V, but I always get the maximum value - 4095.
I am using this code that I saw in the ST examples.

 HAL_GPIO_WritePin(ADC_OUT_GPIO_Port, ADC_OUT_Pin, GPIO_PIN_SET);
 HAL_Delay(50);

 if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) != HAL_OK)
 {
	 Error_Handler();
 }

 if (HAL_ADC_Start_DMA(&hadc1, (uint32_t*)aADCxConvertedData, BATTERY_ARRAY_SIZE) != HAL_OK) {

	 HAL_GPIO_WritePin(ADC_OUT_GPIO_Port, ADC_OUT_Pin, GPIO_PIN_RESET);
	 Error_Handler();
 }

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) {
 if(hadc->Instance == ADC1) {

 if (HAL_ADC_Stop_DMA(&hadc1) != HAL_OK) {
 	Error_Handler();
 }
 HAL_GPIO_WritePin(ADC_OUT_GPIO_Port, ADC_OUT_Pin, GPIO_PIN_RESET);
 uint32_t sum_mv = 0;
 for (uint32_t i = 0; i < BATTERY_ARRAY_SIZE; i++) {
 aADCxConvertedData_Voltage_mVolt[i] = __ADC_CALC_DATA_VOLTAGE(VDDA_APPLI, aADCxConvertedData[i]);
 sum_mv += aADCxConvertedData_Voltage_mVolt[i];
 }

 uint16_t avg_mv = sum_mv / BATTERY_ARRAY_SIZE;

 ubDmaTransferStatus = 1;
 }
}

I put a breakpoint on ubDmaTransferStatus and see what it measures.

I use this same code on the nucleo board by shorting PC1 and PC0 with a wire and seeing normal results, around 3294-3296 mV.

This is not a hardware problem, I measured the output of the divider on the pin with an oscilloscope and saw around 2V. I also tested it on two devices.

I attach a project that works with nucleo, maybe this will help somehow.
Please help me.
Regards.

This topic has been closed for replies.
TDK
TDKBest answer
May 13, 2025 4:52 PM UTC

> It's internally connected to the VDDA.

It is not internally connected to VDDA, it is a distinct pin and must be powered.

That is the root of your issues.

 

Your options are:

  • Modify the hardware to connect VDDA to VREF+.
  • Use VREFBUF to supply a 2.5 V reference. This is the highest voltage it can supply.
"If you feel a post has answered your question, please click ""Accept as Solution""."

19 replies

raptorhal2
Lead
May 13, 2025 2:15 PM UTC

Step through the program in debug mode and see where it goes wrong.

IlliaGxAuthor
Associate III
May 13, 2025 3:08 PM UTC

Hello. Thank you for your answer.
Could you please tell me what I should be looking at? I am already looking at the result in the HAL_ADC_ConvCpltCallback completion callback

Andrew Neil
Super User
May 13, 2025 2:17 PM UTC

@IlliaGx wrote:

 custom board with the STM32WB55 chip..


It's a custom board - so you need to show the schematic.

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
IlliaGxAuthor
Associate III
May 13, 2025 2:57 PM UTC

IlliaGx_0-1747148211647.png

 

Andrew Neil
Super User
May 13, 2025 3:06 PM UTC

You need to show the full schematic!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.