Point to point communication between B-L072z LRWAN1 nodes.
Hi all,
I am new to Lora technology and need some guidance from experts here.I am working on B-L072z LRWAN1 module that allows to transmits messages using Lora. I was able to download and flash the example code available in LRWAN library provided by ST. I can see the messages going out using LED indicator on device as i still don't have my gateway working.I had couple of questions here.
1)can i use two B-L072z LRWAN1 devices to achieve point to point communication using Lora?
2)if yes,how can i achieve that?Is there any example code for that or i need to change the current example i am using to achieve what i want ?
3)My assumption is that if i transmit the message from one device,it should be received by second device.Is my assumption correct?
any help will be appreciated.
Thanks