Skip to main content
EFran.1
Visitor II
Jan 27, 2021 9:16 AM UTC
Question

PLL, cannot reach 48-MHz

Dear all,

I am trying to set-up the internal PLL for running @ 48-MHz.

I can easily set-up the clock tree to achieve frequencies lower than 44-MHz, but when I try 48-MHz, the cpu does not end from the loop that verify that the PLL is OK.

The FLASH is set with 2 WS.

I routed on the MCO the cpu clock and it is correctly set @ 48-MHz

Here is my PLL initialization

​

...

// For f(ck in) = 16-MHz (HSI16)

// f(out) = f(vco) / R f(out) = 48-MHz, R = 4 ---> f(vco) = 192-MHz

// f(vco) = f(ck in) * (N/M) N/M = 48/4 = 12 ---> N = 48, M = 4

// f(rng) = f(vco) / Q Q = 4 ---> f(rng) = 49.5-MHz

// f(adc) = f(vco) / P P = 4 ---> f(adc) = 49.5-MHz

​

RCC->PLLCFGR = ((4-1)<<29) // R = 4

| (1<<28) // PLLR enabled

| ((4-1)<<25) // Q = 4

| (1<<24) // PLLQ enabled

| ((4-1)<<17) // P = 4

| (1<<16) // PLLP enabled

| (48<<8) // N = 48

| ((4-1)<<4) // M = 4

| (2<<0); // HSI16 as a PLL source

​

RCC->CFGR = (0<<28) // MCO (no division)

 | (5<<24) // PLLR output

 | (0<<11) // APB2 bus @ 41.6/1 = 41.6-MHz

 | (0<<8) // APB1 bus @ 41.6/1 = 41.6-MHz

 | (0<<4) // HPRE bus @ 41.6-MHz

 | (3<<0); // PLL selected as a system clock

​

// PLLQ for RNG, ..., PCLK (48-MHz) for ...

​

RCC->CCIPR = (0<<30) // RNG clocked by PLLQ

| (2<<28) // ADC clocked by OPLP

| (0<<22) // LPTIM3 clocked by PCLK

| (0<<20) // LPTIM2 clocked by PCLK

| (0<<18) // LPTIM1 clocked by PCLK

| (0<<16) // I2C3 clocked by PCLK

| (0<<14) // I2C2 clocked by PCLK

| (0<<12) // I2C1 clocked by PCLK

| (0<<10) // LPUART1 clocked by PCLK

| (1<<8) // SPI2 clocked by PLLQ

| (0<<2) // USART2 clocked by PCLK

| (0<<0); // USART1 clocked by PCLK

​

// Enable PLL

// Waiting for the PLL lock

​

RCC->CR |= RCC_CR_PLLON;

while ((RCC->CR & RCC_CR_PLLRDY) == 0);

​

// I can reach this point

​

RCC->CFGR |= RCC_CFGR_SW;

while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS);

​

// ... but I never reach this point for 48-MHz

​

...

​

Any glues to solve my problem?

Best regards

Edo

This topic has been closed for replies.