Skip to main content
NakornThree
Associate II
Jan 1, 2021 7:09 AM UTC
Question

Please suggest Loss communication issues when having many devices in a network.

I developed a LoRa device with STM32L072RZ+SX1272MB2xAS. The device could send data every 40 s and It's working well. But the problem happened when a Lora network has devices with more than 10 nodes. The problem is sometimes devices can't send any data to a server for an hour and it happens at random times and on random devices.

What is the cause of the problem and how to solve it?

This topic has been closed for replies.

4 replies

Vangelis Fortounas
Associate II
Jan 1, 2021 8:45 PM UTC

Hello .

It seems like packet collision issue. I supose that the server is not acts as a coordinator but as a simple receiver. At least a CCA Clear Channel assessment protocol must be implemented.

NakornThree
Associate II
Jan 2, 2021 2:45 AM UTC

Thank you, Vangelis. What is a CCA Channel assessment protocol and how to use it?

Tesla DeLorean
Guru
Jan 2, 2021 3:25 AM UTC

Google is your friend... http://www.wirelesscommunication.nl/reference/chaptr01/wrlslans/80211_page2.htm

Basically you're going to have to tread more carefully so your own transmission aren't treading on top of each other, perhaps via time displacement, or random back-off. If reporting GPS/GNSS positions, there gets to be a unintended synchronization to top-of-second, you need to manage that.

Also the medium is generally half-duplex, so you can jam it in either direction.

LoRa or LoRaWAN ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..