Skip to main content
Aku
Associate II
Feb 5, 2021 3:40 PM UTC
Question

Permanently damaged Radio RX path on STM32WB55

Hi,

we've been developing with stm32wb55 for some time and found that some combinations of STOP2 and radio usage causes permanent damage to RX path.

It looks like that: device announce stops at some point and power consumption raises(+10mA). After reset device starts announce again, but doesn't receive anything.

Flashing TransparentVCP and checking RX with CubeMonitorRF shows RSSI -108dBm

Wiping flash and re-flashing radio and firmware doesn't help.

Overall we've been following all application notes on power, radio, LSE/HSE. The only significant difference is antenna(we use IMD by Ethertronics/AVX 1001312) and software(we use STOP2 in between announces and prevent sleep only when connection arrives).

Disabling STOP2 prevents damage, but completely unacceptable in terms of UX and power consumption.

Since radio is a black box we are completely puzzled by this behavior and were unable to trace cause of damage.

Is there any way to examine radio path internals (like on st25)? As I understand AT0, AT1 exists exactly for that purpose.

Or any other ways to find what may cause RX path damage?

This topic has been closed for replies.

14 replies

Remi QUINTIN
ST Technical Moderator
Feb 11, 2021 10:58 PM UTC

​Yes. Your issue is now investigated by the American region.

Case 00125384 is being handled by the RF team in US. 

They should be your first level contact now.

Msafa.1
Associate II
Feb 26, 2021 9:14 PM UTC

Hi @Remi QUINTIN​ , @Aku​  @Pavel Zhovner​ 

We seem to have the exact same problem here, the RX path is permanently damaged. can we also be included in the discussions? we are also just about to introduce a product to market at large volumes...

Aku
AkuAuthor
Associate II
Feb 27, 2021 10:48 AM UTC

Hi,

sad to hear that. You can open new support case and refer to 00125384, so they can join our issues together.

Here is what we know:

  • Looks like some kind of condition race in core2 firmware
  • Happens when IP_CORE_LP_STATUS and PES_ACTIVITY led is on (try to enable it in app_debug.c and confirm that you have it)
  • Power consumption increase and depends on SMPS status (+5mA if enabled, +10mA if not)
  • It takes time to do the real damage after core2 arrives to this state
  • Arriving to this state correlates with stop mode usage, but not limited to it.
  • With some probability damage happens only in stop mode.

ST Support recommendations:

Also we can make discord/slack/email channel to discuss this issue, drop me a private message if you'd like to participate

Msafa.1
Associate II
Feb 27, 2021 11:03 AM UTC

Thanks @Aku​ , just sent you a private message.