Skip to main content
DS.4
Senior
Oct 18, 2022 9:08 AM UTC
Question

Pairing Authentication for Client (Centaral) side

What parameters of 'aci_gap_set_authentication_requirement' are relevant for client side?

What can I set the irrelevant parameters to?

tBleStatus aci_gap_set_authentication_requirement( uint8_t Bonding_Mode,
 uint8_t MITM_Mode,
 uint8_t SC_Support,
 uint8_t KeyPress_Notification_Support,
 uint8_t Min_Encryption_Key_Size,
 uint8_t Max_Encryption_Key_Size,
 uint8_t Use_Fixed_Pin,
 uint32_t Fixed_Pin,
 uint8_t Identity_Address_Type )

Thanks

This topic has been closed for replies.

1 reply

Remy ISSALYS
ST Technical Moderator
Oct 19, 2022 12:24 PM UTC

Hello,

The same parameters as on server side are relevant for aci_gap_set_authentication_requirement command, you can look in BLE_HeartRate example to see how this command is used.

Best Regards