Skip to main content
Associate II
Sep 6, 2025 1:05 AM UTC
Solved

P-Nucleo-WB55 Low power examples

Hello
I was developing an application that uses BLE and low power mode. I was testing that on a custom board and when I measured the current consumption at STOP2_MODE, it was 1.7 mA.
I expected that I had made a mistake. So I tried the low power examples found there STM32CubeWB/Projects/P-NUCLEO-WB55.Nucleo/Examples/PWR at master · STMicroelectronics/STM32CubeWB on my board and then using the P-Nucleo-WB55 and I found the current consumption is above 4 mA.
Shouldn't be measured in micro-ampere? I am confused now, as I am using an ST example and a dev board, so it should work well.

Thanks in advance.

 

Best regards,

Mahmoud A.

FilipKremen
FilipKremenBest answer
ST Employee
Sep 16, 2025 12:21 PM UTC

Hello,

before measurement with NucleoWB55 please remove everything from JP5 and JP2, also remove USB cable from ST-Link during measurement.

Please let me know if you can reach the stop mode current, thanks.

Best regards,

Filip Kremen

 

3 replies

Associate II
Sep 12, 2025 1:12 PM UTC

?

FilipKremen
FilipKremenBest answer
ST Employee
Sep 16, 2025 12:21 PM UTC

Hello,

before measurement with NucleoWB55 please remove everything from JP5 and JP2, also remove USB cable from ST-Link during measurement.

Please let me know if you can reach the stop mode current, thanks.

Best regards,

Filip Kremen

 

Associate II
Dec 2, 2025 5:51 AM UTC

Hello @FilipKremen,
Yes, it solved the problem. 
Thanks for your help.