Skip to main content
WWU.807
Associate II
October 30, 2019
Question

P-NUCLEO-WB55 does not working on DFU mode

Hi, All,

​

I want to use CubeMon-RF to monitor the USB dongle of the P-NUCLEO-WB55.

According to the Manual : STM32CubeMonitor-RF software tool for wireless performance measurements,

The USB dongle must be monitored using the VCP DEVICE link, and it need to update Firmware to use the example : ble_transparent_mode_vcp.

​

To update the USB dongle's firmware, I must use STM32CubeProg tool.

According to the manual : STM32CubeProgrammer software description,

USB dongle must use DFU mode for Firmware update, and I install DFU driver follow the Chapter 1.2.4.

And set the DFU mode according to this web page https://visualgdb.com/tools/STM32WBUpdater/connecting/.

​

However, when the device is plugged into the PC, the Window Device Manager does not detect any device, and the USB dongle is the same as STM32WB Nucleo.

And Win7 is the same as Win10.

May I ask how to solve this?

​

Thanks. ​

​

This topic has been closed for replies.

47 replies

Remi QUINTIN
ST Technical Moderator
October 30, 2019

​First check: Did you set the switch to the right position on the dongle=> opposite to the USB conector to set BOOT0 option byte to 1. This will set the USB in DFU mode.

WWU.807
WWU.807Author
Associate II
October 30, 2019

Yes, I follow this web page https://visualgdb.com/tools/STM32WBUpdater/connecting/

to set BOOT0 option.

Remi QUINTIN
ST Technical Moderator
October 30, 2019

Then the CubeProgrammer tool should detect it when you select the USB mode​. Check the connection selecting the DFU mode and then click on the "connect" button.

In the end download the BLE_TransparentModeVCP_reference.hex binary at 0x08000000.

WWU.807
WWU.807Author
Associate II
October 30, 2019

Hi, Remi,

​

CubeProgrammer tool in USB mode have no DFU detected.

Remi QUINTIN
ST Technical Moderator
October 30, 2019

​Are you able to detect the Nucleo board in DFU mode?

Remi QUINTIN
ST Technical Moderator
October 30, 2019

​You can also check if the USB device is OK by opening the device manager.  The USB device should be recognized a Boot Loader. See picture.

WWU.807
WWU.807Author
Associate II
October 31, 2019

Dear Remi,

I can't detect USB dongle or ucleo board in DFU mode, The Device manager was no respond when i  plugged USB device in DFU mode.

Remi QUINTIN
ST Technical Moderator
October 31, 2019

Ok let's focus on the Nucleo Board. The document you read looks correct for a NUcleo board. So in the end your board should be configured like the picture below.

Beware to plug your USB wire in the right USB connector (not the ST LINK one).

Then You should se it with the CubeProgrammer tool.

For the Dongle, check the other picture

Then You should se it with the CubeProgrammer tool.

Remi QUINTIN
ST Technical Moderator
October 31, 2019

..

WWU.807
WWU.807Author
Associate II
November 1, 2019

Dear Remi,

I tried to set DFU mode again on Nucleo Board and USB dongle , it still nothing to detected on  CubeProgrammer tool or Windows Device Manager.

Stecklo
Senior
November 6, 2019

I've met this problem yesterday. For me the reason was the nSWBOOT0 option byte set to 0, so the hardware BOOT0 switch does no change. The only way to fix this is to use SWD to program nSWBOOT0 to 1

WWU.807
WWU.807Author
Associate II
November 4, 2019

if the DFU Mode problem can't solved, May I use on board st-link of NUcleo board to update  Nucleo Board & USB Dongle both firmware? Have any document to descrip it?

Thanks a lot.

Remi QUINTIN
ST Technical Moderator
November 4, 2019

​It would be strange you get the same issue on both the nucloeo board and the dongle!!!

I dont know what to propose except using the JTAG/SWD port for the Nucleo board but this is of no use for the dongle.

WWU.807
WWU.807Author
Associate II
November 5, 2019

Dear Remi,

​

I connect JP5 DEBUG pins of Nucleo Board to CN1 DEBUG pins of USB Dongle, then use STM32cubePorg tools to Update Firmware.

​

When I use the example firmware: ble_transparent_mode_vcp, and connect USB Dongle on STM32CubeMoniter-RF.

It show a waring message : "Device Under the test no responing COM port closed"

​

0690X00000Arg3mQAB.png

​

When I update back to demo example: BLE_p2pClient.

Then STM32cubePorg show a error message :"NO STM32 target found"

​

0690X00000Arg5EQAR.png

​

May I ask how to fix those problem?

Thanks.

Remi QUINTIN
ST Technical Moderator
November 6, 2019

​Indeed but when the USB DFU mode is used this nSWboot option byte is set to 1 with the command. Moreover the start of the issue was the USB device not detected.

Anyow it is worth the trial.

If you are able to connect with the JTAG/SWD port then you can either set nSWBOOT0 to 1 as the switch setting the PH3/BOOT0 pin is properly positionned.

launching the command STM32_Programmer_CLI.exe -c port=swd mode=UR -ob nSWboot0=1

or you can launch the command  STM32_Programmer_CLI.exe -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 regardless of  the PH3 BOOT0 pin.

or directly launch the complete command

STM32_Programmer_CLI.exe -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade %FW% %ADDRESS%