P-NUCLEO-LRWAN2 - Sensor-board trouble with AT commands
Following section 4 in UM2587, I've connected an FTDI UART-RS232 adapter to the I-NUCLEO-LRWAN1 sensor board to read the APPEUI but I don't get any response. I've also tried reading from memory 0x08080000 of the NUCLEO-L073RZ board, but I only get zeros. I've tried flashing the L073RZ with the AT_Master demo project from the STM32CubeExpansion_LRWAN_V2.1.0 firmware, following UM2073, but It's still not working.
Should I be able to use AT commands via UART on LPUART1_Rx/Tx independent of the firmware on the NUCLEO-L073RZ ? What changes do I need to make to the AT_Master project to make it work ? I think the AppEUI for example, should be populated automatically into memory based on internal memory of the I-NUCLEO-LRWAN1 ? Or do I need to call the functions LoRa_SetDeviceID() and LoRa_SetAppID() to populate memory 0x08080000 on the L073 ?
I think the documentation could be more "beginner friendly" as most people buy demo-kits to get a minimum working example that you can mess with as an introduction to the technology :(