Skip to main content
Associate II
Aug 6, 2025 12:46 AM UTC
Question

Overrun Errors While Sending Data Through the Radio on STM32WLE5 board

Hello, I have modified the SubGHz_Phy_PingPong example to create separate transmitter-only and receiver-only code for two STM32WLE5 modules.
I'm using the Low Level (LL) driver with UART1 interrupts on the STM32WLE5 TX module to receive data via UART, which is then transmitted over the radio. On the receiving end, the STM32WLE5 module receives the data via radio and forwards it to the target device through UART.

Setup:
UART ---> STM32WLE5 TX------| ( Radio ) |----------- STM32WLE5 RX ------> UART

All data received by the STM32WLE5 TX module is handled exclusively through UART interrupts. Therefore, if interrupts are disabled, the UART will not be able to read any incoming data.

In the STM32WLE5 transmitter code, Radio.Send() disables interrupts while transmitting data over the radio. During this period, UART interrupts are also disabled, preventing UART from receiving incoming data, which leads to overrun errors.

Is there any possible way to prevent UART overrun errors when interrupts are disabled during Radio.Send()?

or Is there a way to keep UART interrupts active while sending data through the radio on the STM32WLE5 module?

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Sep 16, 2025 1:19 PM UTC

Hello @sandeep_kumar_v 

To prevent UART overrun errors on the STM32WLE5, you can enable the OVRDIS bit in the USART_CR3 register. Setting the OVRDIS bit in the USART_CR3 register ensures that new data overwrites the previous content in the LPUART_RDR register without setting the overrun error flag (ORE).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.