Skip to main content
SWent.1
Associate
Aug 5, 2025 11:45 PM UTC
Question

openocd is not working with STM32WBA65 CPU

The bottom line is the  "wba" file stm32wbax.cfg is missing from openocd

Here are the details:

  • I have designed a board with the STM32WBA65 CPU.
  • I downloaded openocd
  • But the needed file stm32wbax.cfg is missing
    • find . -name "stm32wb*"
      ./tcl/target/stm32wbx.cfg


What I need is an openocd that works with the stm32wbax.cfg file.
I have found the file in https://github.com/openocd-org/openocd 
However, that file does not work with openocd distributed by MorseMicro

  • openocd --version
    xPack Open On-Chip Debugger 0.12.0+dev-01312-g18281b0c4-dirty (2023-09-04-22:31

And I built openocd from scratch and it also fail

  • openocd --version
    Open On-Chip Debugger 0.12.0-rc3-00999-gfcb40f49b (2025-08-05-13:39)

Conclusion: 

When you find the file stm32wbax.cfg, please make sure it works with openocd.

And please add LABELS to your GUI so I can file under STM32WBA or STM32WBA65

 

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
Sep 16, 2025 4:03 PM UTC

Hello @SWent.1 

Could you please give more details about what is not working exactly and what is your test process.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Oct 10, 2025 9:42 PM UTC

I have the same issue, I can not get mainline top of tree regular openocd or ST fork of openocd to work with STM32WBA65.   

For regular openocd:

    clone: https://github.com/openocd-org/openocd.git

    hash:  896738264e92b74a17250dab639999a2743d0b7c  from 9/27/2025

For st fork

    clone: https://github.com/STMicroelectronics/OpenOCD.git

    hash: 0de861e21c12fd39fdce7b6296994d89eca6146f from 12/03/2024

Regular openocd

When I run openocd with the following command-line it appears to work at first:

~/repos/openocd/src/openocd -s ~/repos/openocd/tcl -f interface/stlink.cfg -f target/stm32wbax.cfg
Open On-Chip Debugger 0.12.0+dev-02228-ge5888bda3 (2025-10-03-23:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Warn : DEPRECATED: auto-selecting transport "swd (dapdirect)". Use 'transport select swd' to suppress this message.
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J16M9 (API v3) VID:PID 0483:3754
Info : Target voltage: 3.267778
Info : Unable to match requested speed 500 kHz, using 200 kHz
Info : Unable to match requested speed 500 kHz, using 200 kHz
Info : clock speed 200 kHz
Info : SWD DPIDR 0x0be12477
Info : [stm32wbax.cpu] Cortex-M33 r0p4 processor detected
Info : [stm32wbax.cpu] target has 8 breakpoints, 4 watchpoints
Info : [stm32wbax.cpu] Examination succeed
Info : [stm32wbax.cpu] starting gdb server on 3333
Info : Listening on port 3333 for gdb connections

However as soon as I attach with gdb

Reading symbols from build/make.elf...
(gdb) target extended-remote localhost:3333
Remote debugging using localhost:3333
Remote communication error. Target disconnected.: Connection reset by peer.
(gdb)

And back in the openocd shell I now see

...  continuing from previous ...

Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: Failed to read memory at 0x40015800
Warn : Cannot identify target as an STM32C0/G0/G4/L4/L4+/L5/U0/U3/U5/WB/WL family device.
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected

ST Fork of openocd

It doesn't contain stm32wbax.cfg so it fails.

~/repos/openocd_st/src/openocd -s ~/repos/openocd_st/tcl -f interface/stlink.cfg -f target/stm32wbax.cfg
Open On-Chip Debugger 0.12.0-00033-g0de861e21 (2025-10-10-14:21) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
embedded:startup.tcl:28: Error: Can't find target/stm32wbax.cfg
in procedure 'script' 
at file "embedded:startup.tcl", line 28
make: *** [Makefile:212: openocd] Error 1

If I try to use stm32wbx instead I get:

~/repos/openocd_st/src/openocd -s ~/repos/openocd_st/tcl -f interface/stlink.cfg -f target/stm32wbx.cfg
Open On-Chip Debugger 0.12.0-00033-g0de861e21 (2025-10-10-14:21) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 500 kHz
Info : STLINK V3J16M9 (API v3) VID:PID 0483:3754
Info : Target voltage: 3.267778
Warn : UNEXPECTED idcode: 0x0be12477
Error: expected 1 of 1: 0x6ba02477

^^^^ this would be expected of an unidentified ID.

Associate II
Oct 10, 2025 10:40 PM UTC

Build a debug version, and stepping in, fundamentally the issue appears to be that even though I specified an stm32wbax.cfg, internally this ends up resulting in a flash "driver" object based on stm32l4.

 

Looking through those sources src/flash/nor/stm32l4x.c, I see mention of:

/* STM32WBxxx series for reference.
 *
 * RM0493 (STM32WBA52x)
 * http://www.st.com/resource/en/reference_manual/dm00821869.pdf
 *
 * RM0434 (STM32WB55/WB35x)
 * http://www.st.com/resource/en/reference_manual/dm00318631.pdf
 *
 * RM0471 (STM32WB50/WB30x)
 * http://www.st.com/resource/en/reference_manual/dm00622834.pdf
 *
 * RM0473 (STM32WB15x)
 * http://www.st.com/resource/en/reference_manual/dm00649196.pdf
 *
 * RM0478 (STM32WB10x)
 * http://www.st.com/resource/en/reference_manual/dm00689203.pdf
 */

/* STM32WLxxx series for reference.
I don't see STM32WBA65 mentioned, so possibly the issue.