Skip to main content
Associate
Oct 29, 2025 8:23 AM UTC
Question

Nucleo WL55JC2 - Generate continuous 432.492 MHz

Hi,

I’m looking for some help — I’m trying to generate a continuous waveform at 432.492 MHz using the Nucleo WL55JC2, but I haven’t had any success so far. I also tried at 861.1 MHz, but still got no output.

After extensive troubleshooting, I discovered that the issue was caused by the TCXO (PB0) not being powered at 3.3 V, and the SP3T not being properly configured because PC3/PC4/PC5 remained at 0 V instead of 3.3 V.

To address this, I modified the project — without generating the CW signal for now — simply to control the state levels of PB0, PC3, PC4, and PC5, and to make it work correctly with both the CM0+ and CM4 cores.


M0PLUS main.c is:

#include "stm32wlxx_hal.h"

static void Error_Handler(void)
{
__disable_irq();
while (1) { }
}

int main(void)
{
HAL_Init();

/* Clocks GPIOB/GPIOC */
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();

/* Configure PB0, PC3/PC4/PC5 en sortie push-pull */
GPIO_InitTypeDef g = {0};
g.Mode = GPIO_MODE_OUTPUT_PP;
g.Pull = GPIO_NOPULL;
g.Speed = GPIO_SPEED_FREQ_LOW;

/* PB0 = VDD_TCXO (SB20 = ON) */
g.Pin = GPIO_PIN_0;
HAL_GPIO_Init(GPIOB, &g);

/* PC3 = VDD_SP3T ; PC4/PC5 = sélecteurs (SB18 = ON) */
g.Pin = GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5;
HAL_GPIO_Init(GPIOC, &g);

/* Force tout à 1 : PB0, PC3, PC4, PC5 */
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5, GPIO_PIN_SET);

/* Boucle vide : les niveaux restent maintenus */
while (1) { __NOP(); }
}

and M4 main.c is
// CM4 main.c (minimal)
#include "stm32wlxx_hal.h"

int main(void)
{
HAL_Init();

// Horloge système basique (ou ta SystemClock_Config existante)
// SystemClock_Config(); // si tu l’as déjà

// Libère le CM0+
HAL_PWREx_ReleaseCore(PWR_CORE_CPU2);

while (1) { __NOP(); }
}


But still not working.
It seem that CM0PLUS is blocked.

The link to the project available 7 days:

https://fromsmash.com/JgyvPbhz4w-ct

Thanks by advance !
Franck


Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

2 replies

Franck95Author
Associate
Nov 3, 2025 6:01 AM UTC

I found a second way to make it works.

 

ST Technical Moderator
Nov 3, 2025 7:20 AM UTC

Hello @Franck95 

I am glad to know that the issue has been resolved.
Please share the solution that you found. Then, close this topic by marking the answer as "Accept as Solution". This action helps other users find the solution more quickly.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks