Skip to main content
Associate
Jan 8, 2026 11:04 AM UTC
Question

NUCLEO-WL55JC1 Sleep Mode Current Consumption

Screenshot 2026-01-08 162641.png

Hi,

I am using the NUCLEO-WL55JC1 board and referring to the PWR_STOP2_RTC example to measure current consumption.

I have isolated the ST-LINK section and am powering the board with an external 3.6 V supply for accurate measurement. However, in sleep (STOP2) mode, the measured current consumption is about 1.64 mA, which seems higher than expected.

Please let me know if this is normal for this configuration or if any additional steps are required to further reduce the current consumption.

5 replies

Gyessine
ST Technical Moderator
Jan 8, 2026 12:52 PM UTC

Hello @Deep23 
First, and just to ensure that there is nothing wrong in your project code.
can you run this firmware example and measure the power consumption?

BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Deep23Author
Associate
Jan 9, 2026 5:00 AM UTC

Hello,

I have run the example firmware (PWR_STOP2_RTC) from the STM32WL SDK as suggested. However, the measured current consumption is still around 1.6 mA in sleep mode. Please find the attached image for reference.

 

Deep23_0-1767934663257.png

 

Gyessine
ST Technical Moderator
Jan 9, 2026 8:50 AM UTC

Hello @Deep23 
Can you explain how you performed the measurement?
Did you measure it through JP1?
I tried the example, and the consumption decreased from several milliamperes to several microamperes when the device entered stop 2 mode.
The firmware is designed to enter sleep mode five seconds after the program starts and remain in sleep mode for 33 seconds.
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Deep23Author
Associate
Jan 10, 2026 12:34 PM UTC

Deep23_0-1768047706765.png

Deep23_2-1768048576044.png

 

Hello,

Please find the attached image showing the current measurement setup for the NUCLEO-WL55JC1 board.
let me know if there is anything incorrect or that needs to be improved.

Regards,
Deep

 

Gyessine
ST Technical Moderator
Jan 12, 2026 4:00 PM UTC

hello @Deep23 
Did you ensure to place the jumpers in their correct new positions after removing them from the STLINK position? because you didn't mention where you placed them.
You can refer to this user manual to see how to configure jumpers for each power source.
Also, as an initial test, first run the test while powering the board from STLINK to ensure that the product can enter stop mode. 
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.