Skip to main content
Visitor II
Jul 30, 2026 2:44 PM UTC
Question

NUCLEO-WL55JC1: LoRaWAN_End_Node_LBM Join Accept Failed with Code 14 (ChirpStack)

Hello ST Community,

I am attempting to run the LoRaWAN_End_Node_LBM example project from the STM32CubeWL MCU Firmware Package on a NUCLEO-WL55JC1 board, connecting to a ChirpStack LoRaWAN Network Server.

While ChirpStack shows both the Join Request and Join Accept frames, the node fails to join and loops endlessly in a join retry state.
Configuration & Keys

    Updated AppEUI in se-identity.h to match ChirpStack settings.

    Tested on STM32CubeWL Firmware Package V1.6.0 (and verified same issue on V1.5.0).

Environment / Software Versions

    Application: LoRaWAN_End_Node_LBM (V1.6.0)

    Middleware (MW) LoRaWAN: V1.1.0

    Middleware (MW) Radio: V1.4.0

    L2 Spec: V1.0.4

    RP Spec: V2-1.0.4


Serial Monitor

188s692: TX DONE

188s739: RX1 LoRa at 4953 ms freq:868300000, DR 4, BW125, rx timeout 16 ms

193s827: RX DONE

193s827: RP: RX size 33

193s828: Process join accept failed with code = 14

193s828:Receive a bad packet on RX1 for stack_id = 0 continue with RX2

193s828: RX2 LoRa at 895 ms freq:869525000, DR 0, BW125, rx timeout 196 ms

194s920: IRQ_RADIO_RX_TX_TIMEOUT

Event received: JOINFAIL

Has anyone encountered Process join accept failed with code = 14 with the LBM stack? Any insights into what error code 14 indicates or suggestions on resolving this would be greatly appreciated.

 

3 replies

RusikOk
Associate III
Aug 8, 2026 6:53 PM UTC

It sounds like this is your situation 

 

ST Technical Moderator
Aug 9, 2026 3:37 PM UTC

Hello ​@gsmith84099 ,

This error code is related to a mismatch on security material between the End-Device and the ChirpStack configuration.

We noticed you changed the AppEUI without specifying the value set.

Could you please share the configuration of JoinEUI ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Aug 17, 2026 10:23 AM UTC

Hi ​@gsmith84099 ,

Do you have update on this issue?

Could you please share your configuration of JoinEUI ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks