Skip to main content
HKhan.4
Associate II
May 21, 2025 7:42 AM UTC
Question

Nucleo-WL55JC1 - Lora Network Time Request

Good day 

 

I am currently trying to run the end_node sample located on the STM32Cube_FW_WL_V1.3.1 package.  I would like to know if i can have some guideline on how to use LmHandlerDeviceTimeReq().  

Which class do i need to use?

What lora server allows the time request?

How do i check if the MAC request is even sending?  Should I see this on the Logs under my application located on the server?

The request currently is not updating my system time.  The request is currently being done in a callback after a successful join. 

static void OnJoinRequest(LmHandlerJoinParams_t *joinParams)

{

/* USER CODE BEGIN OnJoinRequest_1 */

if (joinParams->Status == LORAMAC_HANDLER_SUCCESS)

{

APP_LOG(TS_ON, VLEVEL_L, "JOINED\n");

 

// Send time request

if (LmHandlerDeviceTimeReq() == LORAMAC_HANDLER_SUCCESS)

{

APP_LOG(TS_ON, VLEVEL_L, "DeviceTimeReq sent.\n");

}

}

/* USER CODE END OnJoinRequest_1 */

}

After the request is sent successfully, the below lines are never run.

static void OnSysTimeUpdate(void)

{

/* USER CODE BEGIN OnSysTimeUpdate_1 */

SysTime_t time = SysTimeGet();

APP_LOG(TS_ON, VLEVEL_L, "Network Time: %lu (UNIX timestamp)\n", time.Seconds);

 

/* USER CODE END OnSysTimeUpdate_1 */

}

My setup is as follows:

HKhan4_0-1747813166952.pngHKhan4_1-1747813210617.png

 

This functionality is crucial to our project .

thank you in advance!

 

2 replies

STTwo-32
ST Technical Moderator
May 21, 2025 5:35 PM UTC

Hello @HKhan.4 

End-devices and Network Servers SHALL implement these commands. This MAC command has been introduced in LoRaWAN L2 1.0.3. An end-device MAY use the DeviceTimeReq command to request the current network time from the Network Server. This allows the end-device to synchronize its internal clock to the Network’s clock. This is specifically useful to speed up the acquisition of the Class B beacon. The request has no payload. A Network Server MAY use the DeviceTimeAns command to provide the GPS time to the end-device. The time provided is the GPS time at the end of the uplink transmission. The command has a 5-octet payload defined as follows:

STTwo32_0-1747848896993.png

The time provided by the Network SHALL have a worst-case accuracy of ±100 ms. The DeviceTimeAns command SHALL be sent as a Class A downlink (i.e., over RX1/RX2 of the Class A mode).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Jan 30, 2026 12:43 PM UTC

Hi,

What is the process to do this? I am trying the same method. I need to receive the time from the network server.