Skip to main content
Associate
Nov 18, 2025 12:28 AM UTC
Question

Nucleo-WL55JC1 Debug Error

I am trying to debug code for Nucleo-WL55JC1 board using sample code from the STM website.  It is the LoRAWAN_End _Node.  I complies fine and creates .elf file.  However when a try do download with the STM32Cube I get the following error:

An internal error occurred during: "Launching LoRaWAN_End_Node".
'com.st.stm32cube.ide.mcu.toolchain.IToolChainInfoProvider[] com.st.stm32cube.ide.mcu.toolchain.ToolChainHelper.getToolChainInfoProviders()'

 

Thanks for the help.

This topic has been closed for replies.

2 replies

ST Technical Moderator
Nov 18, 2025 7:04 AM UTC

Hello @jlaiosa 

Please provide more details: STM32CubeIDE version, Java runtime version, exact steps you perform when launching debug, 

Make sure to use latest releases of STM32CubeMX/CubeIDE.

Perform a Project > Clean to remove all build artifacts, rebuild the project fully. Then try launching the debug session again.

If you import the project, follow this article and make sure to use the latest release of STM32CubeMX/IDE as contains limitations fixes: How to import STM32CubeWL repository projects onto different packages

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
jlaiosaAuthor
Associate
Nov 18, 2025 5:09 PM UTC

STM32CubeIDE

 

Version: 1.19.0

Build: 25607_20250703_0907 (UTC)

 

(C) 2025 STMicroelectronics ALL RIGHTS RESERVED

 

STM32CubeMX - STM32 Device Configuration Tool

 

Version: 6.15.0-RC7

Build: 20250701-1659 (UTC)

 

Copyright (c) 2025 STMicroelectronics. All rights reserved

 

Cannot find java runtime.

 

The procedure is as follows:

- Clean

- Build

- Debug as a C/C++ Application


jlaiosa_2-1763485706997.png

 

 

jlaiosa_3-1763485736948.png