Skip to main content
Associate II
May 25, 2025 3:19 PM UTC
Solved

NUCLEO-wl55jc StandBy mode

Hello everyone !

I'm currently working on the STM NUCLEO-wl55jc card and I'm having a few problems with it.
I'm using the Ping Pong example code, which allows LoRa point-to-point communication between 2 cards. This works perfectly.
My problem now is that I'd like to put one of my 2 cards in StandBy mode. So I use the function ‘HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1_HIGH);’ -> line 113, to initialise the wakeup pin, and the function ‘HAL_PWR_EnterSTANDBYMode();’ -> line 117, to enter StandBy mode. Then, in my while(1) loop, under ‘ifdef GO_TO_LOW_POWER’, I simply want to turn on an LED when I exit StandBy mode and start LoRa communication using this ‘MX_SubGHz_Phy_Process();’ -> line 146, function. However, when a pulse arrives on the wakeup pin, PA0, the LED lights up but unfortunately communication doesn't take place. So I wanted to know if this was the right way to proceed and if my card really went into StandBy mode at the start or not. Because when it's supposed to be in this mode, 2 LEDs are lit on the card, which I find strange.

In addition, I power my board in STD_5V_ALONE mode, so only the MCU, and I measure the current directly on jumper JP1, to get an idea of the current consumed by the processor and I measure around 8mA. I noticed that if I removed this line "MX_SubGHz_Phy_Init();" -> line 96, the consumption fell to 0mA, which could correspond to the StandBy current, I don't really know. Perhaps the call to this function is preventing my card from entering StandBy mode? I'm a bit at a loss here.
I'm sharing my main.c with you so that you can get a better idea of my problem.

For information, to download the code onto my card, I do a ‘build’ and then a ‘run’ for each of my cards.
If anyone could help me it would be a great pleasure.

Thanks in advance !

KYZ.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2021 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "app_subghz_phy.h"
#include "gpio.h"


/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */



int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 //Test
 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();


 //Initialize LoRa communication
 MX_SubGHz_Phy_Init();


 /* USER CODE BEGIN 2 */
/*------------------------------------------------------------
//Code permettant de switcher entre les 2 cartes différentes
------------------------------------------------------------*/



 #ifdef GO_TO_LOW_POWER	//Carte LOW_POWER


	 //Clear previous flags
	 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

	 //Activate the wakeup pin
	 HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1_HIGH);


	 //Enter StandBy mode
	 HAL_PWR_EnterSTANDBYMode();

 #else	//Carte normale

 #endif
/*------------------------------------------------------------
 --------------------------------------------------------------
 ------------------------------------------------------------*/



 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	#ifdef GO_TO_LOW_POWER		//For the low power card which is in StandBy mode

	 //Used to check whether or not you are coming from STANDBY mode
	 if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
	 {
		 //The card has woken up from STANDBY
		 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // Nettoyer le flag

		 //The LED lights up when you exit STANDBYL modeThe board has woken up from STANDBY
		 HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET); // Allumer la LED
		 
		 //To start the PingPong between the two cards (LoRa)
		 MX_SubGHz_Phy_Process();
		 
	 }

	#else		//For the another card
	 	HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET); //LED on
	 	HAL_Delay(200);
	 	HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET); //LED off
	 	HAL_Delay(200);
	#endif


 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_11;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK3|RCC_CLOCKTYPE_HCLK
 |RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
 |RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK3Divider = RCC_SYSCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 while (1)
 {
 }
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 25, 2025 8:48 PM UTC

On the Ping Pong example, this utility is already implemented to enter end exit low power modes will no activity (of printing or dma or send and receive or others). The low power mode can be sleep stop or standby. This utility is used to make it easy to configure and access the Low power modes on a Wireless context that is based on a sequencer and other utilities. So, just have a look at the configuration of your application and the description on the application note I’ve already recommandes to you. It should help you to configure LoRa apps with all needed features. For the HAL_PWR_EnterSTANDBYMode(), it is a function used to entre StandbyMode as well. It can be used on the wireless context but you should take care of the different functions of the application. Debugging the ping pong app should give you more details also. Also, you can take a look at this video to understand the full P2P configuration.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

STTwo-32
ST Technical Moderator
May 25, 2025 3:43 PM UTC

Hello @KYZ 

On the STM32WL LoRa context, for low power modes. You can use the functions of the Tiny_LPM utility so you can enable and disable low power modes (sleep, stop and off modes). More details are available on the AN5406 and specially on the chapter 9.3.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KYZAuthor
Associate II
May 25, 2025 7:25 PM UTC

Hello @STTwo-32,
Thank you for your quick response. So if I understand correctly, I need to call the "PWR_EnterOffMode" function, which will allow me to enter Standby mode (low power consumption). But is the function I was using previously, namely "HAL_PWR_EnterSTANDBYMode();," correct? Because for me, this function should allow me to enter Standby mode, right? I don't really understand why I would use one function or the other.

Best regards

KYZ

STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 25, 2025 8:48 PM UTC

On the Ping Pong example, this utility is already implemented to enter end exit low power modes will no activity (of printing or dma or send and receive or others). The low power mode can be sleep stop or standby. This utility is used to make it easy to configure and access the Low power modes on a Wireless context that is based on a sequencer and other utilities. So, just have a look at the configuration of your application and the description on the application note I’ve already recommandes to you. It should help you to configure LoRa apps with all needed features. For the HAL_PWR_EnterSTANDBYMode(), it is a function used to entre StandbyMode as well. It can be used on the wireless context but you should take care of the different functions of the application. Debugging the ping pong app should give you more details also. Also, you can take a look at this video to understand the full P2P configuration.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.