Skip to main content
MKoca.1
Senior
Nov 11, 2021 8:26 AM UTC
Solved

NUCLEO WL5 debug problem

Hello to everyone. I am trying to develop an application on Lora on the NUCLEO WL5 series development board. But I could not debug the board via CubeMx. I am trying to use external debugger but I still have mcu not found problem. Can anyone tell me how to make ST_LINK debugger connections with WL5?

This topic has been closed for replies.
YBOUV.1
YBOUV.1Best answer
ST Employee
Nov 12, 2021 8:24 AM UTC

Hi @MKoca.1​ ,

If you want to debug, you need to set in sys_conf.h

#define DEBUGGER_ENABLED      1

#define LOW_POWER_DISABLE     1

let me know if this is ok for you

5 replies

Markus GIRDLAND
ST Employee
Nov 11, 2021 9:53 AM UTC

Hello there!

CubeMX doesn't have any debugging capability. It's made to generate code.

Can you find the MCU if you use the regular debugger in STM32CubeIDE? Or if you try to connect to the MCU through CubeProgrammer?

You can see the command line used by going to the debug configuration and you can find more information about how to connect to a remote GDB server by reading the ST-LINK GDB server manual (UM2576) and there's some additional information about the debug flow and how to set up STM32CubeIDE available in the STM32CubeIDE user guide (UM2609).

MKoca.1
MKoca.1Author
Senior
Nov 11, 2021 10:55 AM UTC

Sorry for mis-explaining. Of course, I'm trying to debug CubeIde. I'm using an external ST_LINK debugger but I still haven't succeeded. I think I made the pin connections between Debugger and Board correctly, but I'm not entirely sure. I would be very grateful if you could help with this. @Markus GIRDLAND​ 

YBOUV.1
YBOUV.1Best answer
ST Employee
Nov 12, 2021 8:24 AM UTC

Hi @MKoca.1​ ,

If you want to debug, you need to set in sys_conf.h

#define DEBUGGER_ENABLED      1

#define LOW_POWER_DISABLE     1

let me know if this is ok for you

MKoca.1
MKoca.1Author
Senior
Nov 15, 2021 12:23 PM UTC

@YBOUV.1​ I did what you said and now I can debug in CubeIDE. But there is something I don't understand. If I do LovePowerDisable 1 the system goes into sleep mode all the time. It says so in the description. I couldn't understand this part.

MKoca.1
MKoca.1Author
Senior
Nov 15, 2021 6:39 AM UTC

@YBOUV.1​  Thank you for your answer. I did what you said. I still can't debug in CubeIDE. I was able to run the project in the "Application" folder in CubeProgrammer. But there is a problem, the HAL_Delay() function does not work. I solved this problem for now by putting a wait with a for loop.