Skip to main content
Senior III
Aug 13, 2026 11:23 AM UTC
Solved

NUCLEO-WB55.USBDongle not advertizing

I’m trying to migrate a project from the P NUCLEOWB55 MB1355 board to the P NUCLEOWB55 MB-1293 USB dongle.

I retargeted the board in MX & check the pinouts etc, all fine. Opened up the project in CubeIDE & built the project.

I then switched the board to BOOT0=0 (SW2) & plug it in & open CubePrg

First issue, its really hit & miss if Prg detects the board. Most often I get Port: No DFU detected but then sometimes I actually get Port: Port 1 and the board can be connected to. It really appears to be pot luck if Prg decides it can connect.

If I do manage to get it to connect, I update the FUS & stack, press the Start Stack button as outlined in a previous question, and continue to upload my *.elf file.

Second issue, I get nothing from the BLE, no advertising at all. This project works fine on the MB-1355 board by the way.

NicRobertsBest answer
Senior III
Sep 1, 2026 9:34 AM UTC

OK got it working, had forgot to update the firmware with the BLE stack!

7 replies

Senior III
Aug 13, 2026 2:04 PM UTC

Update (as there doesn’t seem to be an option to edit the OP) Figured out the Prg USB issue switch BOOT0=1 (SW2 to the right) prior to insert then start Prg.

Still nothing from the dongle though. I added some code to turn on the blue LED but that doesn’t light up either. Prg assures me that the firmware was uploaded though…. puzzling…

The board is seen as “DFU in FS Mode” by Windows when BOOT0=1 but is completely ignored when BOOT0=0

 

/* Blue LED on inside main() */
RCC->AHB1ENR |= (1U<<0);
GPIOA->MODER |= (1U<<8);
GPIOA->MODER &=~(1U<<9);
GPIOA-ODR |= (1U<<4);

 

ST Employee
Aug 24, 2026 11:05 AM UTC

Hello ​@NicRoberts, 
SW2 switch is used to choose whether to upload new firmware or to run the user firmware.

When BOOT0=0, the dongle runs user firmware after reset and therefore Windows ignores it correctly.
When BOOT=1, USB bootloader is enabled and you are able to upload new firmware. 

So, you need to switch BOOT0 to 1, upload your project, then switch BOOT0 to 0 and reset the dongle.

For more information, please refer to UM2435.

If you have any further question, do not hesitate to ask

Best Regards,

grohmano

Senior III
Aug 24, 2026 11:41 AM UTC

Hi, I worked out the BOOT0 options and Prg assures me that the code has been uploaded. Its still not advertising its BLE service though. From what I understand the board should be getting power via the USB regardless of the position of the BOOT0 switch but I cant even get an LED to light up never mind broadcasting over BLE.

ST Employee
Aug 24, 2026 12:18 PM UTC

Yes, you are right. The board is powered through USB regardless of BOOT0 switch. 

BOOT0 only selects which firmware is executed after reset:

  • =0 - bootloader/DFU mode
  • =1 - user firmware

To determine whether the problem is in project migration or it is hardware issue, you can flash the BSP example from Cube package and see if LEDs are blinking

 

NicRobertsAuthorBest answer
Senior III
Sep 1, 2026 9:34 AM UTC

OK got it working, had forgot to update the firmware with the BLE stack!