Not generating PWM signal after wake up from STOP2
I'm working with STM32WL and trying to be able to generate PWM signal after wake up from STOP2 to control RGB LED. Before going to STOP2 I deinitialize PWM channel pin and disable timer clock. MCU wakes up on button press. After wake up timer clock is beeing enabled and channel pin is reinitialized. Despite that the LED is off. What else should I do to make it work or what I've done wrong?
/* USER CODE BEGIN 2 */
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Green LED on */
HAL_TIMEx_PWMN_Start(&htim16, TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 1000);
HAL_Delay(500);
/* DeInit of LED pin, disable TIM16 clock */
HAL_TIMEx_PWMN_Stop(&htim16, TIM_CHANNEL_1);
HAL_GPIO_DeInit(LED_G_CH_GPIO_Port, LED_G_CH_Pin);
__HAL_RCC_TIM16_CLK_DISABLE();
/* Enter STOP2 */
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
/* Wake up from STOP2 on button press */
SystemClock_Config();
HAL_ResumeTick();
/* Enable TIM16 clock */
__HAL_RCC_TIM16_CLK_ENABLE();
/* ReInit of LED pin */
__HAL_RCC_GPIOB_CLK_ENABLE();
GPIO_InitStruct.Pin = LED_G_CH_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF14_TIM16;
HAL_GPIO_Init(LED_G_CH_GPIO_Port, &GPIO_InitStruct);
/* Green LED on */
HAL_TIMEx_PWMN_Start(&htim16, TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 1000);
/* USER CODE END 2 */