Skip to main content
Associate III
May 12, 2026 7:32 AM UTC
Solved

Non standard preamble on STM32WL33

I need to implement a protocol using 11110000 as preamble. The protocol is 2-FSK 868.1 MHz, +/-35kHz, 25kbps. According to RM0511 STM32WL33 only supports 01010101 or 10101010 as preamble for 2-FSK. Is it feasible to use the STM32WL33? I am planning to use direct buffer mode.

Filippo_MalleoBest answer
ST Technical Moderator
May 12, 2026 4:08 PM UTC

Hi DirkH, 

yes, you can use the Direct through buffer mode, so you can implement your protocol bypassing any packet handler constraint.

BR,
Filippo

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Filippo_MalleoBest answer
ST Technical Moderator
May 12, 2026 4:08 PM UTC

Hi DirkH, 

yes, you can use the Direct through buffer mode, so you can implement your protocol bypassing any packet handler constraint.

BR,
Filippo

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks