Skip to main content
Associate II
May 13, 2025 2:13 AM UTC
Question

No VCP response on pushing B2 button with MRSUBG_WakeupRadio_Tx example

example code : MRSUBG_WakeupRadio_Tx of STM32Cube_FW_WL3_V1.1.0

board : NUCLEO-WL33CC1

compiler : Keil

running the code, at first message below will shown on Virtual Com,

"STM32WL3 LPAWUR - Transmitter example.
Use PUSH Button 2 to send a frame."

but after pushing Button 2 on board, no message is shown on Virtual Com?!

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
May 26, 2025 3:57 PM UTC

Hello @Gwo 

Behavior reproduced and escalated internally for review on the future (Under internal ticket number 210819). For now, you can still use the Version throw the STM32CubeIDE.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.