Skip to main content
Kampi
Associate III
Feb 16, 2024 5:42 AM UTC
Solved

No SubGHz interrupt on STM32WLE

I use a RAK3172 module for a 434 MHz LoRa APRS application but I don´t get a SubGHz interrupt during transmission. The output from my code is the following:

APRS Demo
Application version: V1.3.0
Radio version: V1.3.0

Radio settings
LoRa Bandwidth: 125 kHz
LoRa Spreading factor: 12
LoRa Frequency: 433775000
Device reset...
Initialization successful!
Go

I tested the code before on an STM32WL Nucleo and there it runs fine. So I think there is some issue with the port to the RAK platform.

I add the link to the GitHub repository so you can checkout the complete codebase because ZIP files aren´t allowed.

https://github.com/Kampi/LoRa-GPS-Tracker/tree/1.1_Dev

Thanks for your support!

This topic has been closed for replies.
Kampi
KampiBest answer
Associate III
Apr 15, 2024 9:41 AM UTC

Hi @STTwo-32 

I already found a solution. It looked like the pinout for the RF switch was wrong. After fixing it everything works smoothly.

6 replies

STTwo-32
ST Technical Moderator
Feb 16, 2024 6:52 AM UTC

Hello @Kampi 

As the problem is on a module that use the STM32WL but it is designed by a third party. 

So, it will be better to ask this question on his forum since everything works fine with the STM32WL.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Kampi
KampiAuthor
Associate III
Feb 16, 2024 11:57 AM UTC

Hi @STTwo-32 

I don´t think it´s a hardware issue because I don´t get a Tx complete interrupt from the SubGHz radio, so the callback isn´t called. So it´s an issue with the STM32WLE.

STTwo-32
ST Technical Moderator
Feb 16, 2024 12:01 PM UTC

You may have to ensure that you have correctly migrated your project to the STM32WLE MCU. Refer to the MCUs datasheets and reference manuals.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.