Skip to main content
JTurn.2
Associate III
Aug 18, 2025 3:47 AM UTC
Solved

No STM32WB0 MCU hardware development application note

Hi everyone,

 

I couldn't find the application note on STM32WB0 MCU hardware development. Can I refer to AN5290 which is for STM32WB instead of the STM32WB0. If so, is there anything I would need to pay attention to for the STM32WB0 series? Or should I reference from the NUCLEO-WB07CC's schematics instead? 

 

Thank you for your time and help!

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 18, 2025 7:02 AM UTC

Hello @JTurn.2 

The AN5290 is applicable only for the STM32WB series. For the STM32WB0, you can use the AN5129, the AN5526 and the design of the STM32WB0 Nucleo boards (NUCLEO-WB05KZ, the NUCLEO-WB07CC, and the NUCLEO-WB09KE. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 18, 2025 7:02 AM UTC

Hello @JTurn.2 

The AN5290 is applicable only for the STM32WB series. For the STM32WB0, you can use the AN5129, the AN5526 and the design of the STM32WB0 Nucleo boards (NUCLEO-WB05KZ, the NUCLEO-WB07CC, and the NUCLEO-WB09KE. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.