Need help related freeRTOS timing mechanism implementation, on BLE P2P Server project, running on STM32WB, instead of existing UTIL_SEQ_Run(~0) timing mechanism
Hello,
I made several modifications to the STM32WB HandsOn_3 example (based on p2p-server project located at c:\STM32WB_workshop\HandsOns\HansdsOn_3) and succeeded to communicate with my mobile application - all OK =)
However the above working solution is based on Sequencer (UTIL_SEQ_Run(~0) ) scheduling mechanism. As my entire project is based on freeRTOS, I'd like to find the best approach on how to convert the working Sequencer mechanism into freeRTOS Mechanism? (for P2P server project)
P.S
- I tried to modified the above working HandsOn_3 project, in CubeMX 5.4 by unchecked the Sequencer utility, and checked the freeRTOS however:
- CubeMX auto code generator implements the HRS one way comm vs. P2P Server two way comm.
- while debug this code in CubeIDE (1.1.0) the FW got stuck in endless loop
2. I checked the example located at: ..\Repository\STM32Cube_FW_WB_V1.3.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRateFreeRTOS
This example works OK, however:
- It is again one way comm. only HRS
- It is based on freeRTOS but the code was generated manually, without CubeMX project file
I need help, to decide which approach will be the best starting point, before FW modification either PS#1 or PS#2 ?
Thanks In Advance,
Micha