Skip to main content
brian239955_stm1
Associate II
Jan 14, 2022 10:16 PM UTC
Question

Need hardware and firmware recommendation for sub-1GHz radio project

Hi,

 I'm starting a new project for a client that needs a sub-1 GHz transmitter and receiver. The distance between the 2 communicating devices will be fixed at approximately 5 ft apart. There will be potential obstructions of metal between the 2 devices. The data to communicate is 1-way only, and is just the value of a switch (open or closed). The receiver needs to detect the switch closing at the transmitter within 100 ms.

 Can you recommend hardware and firmware (including starting example code) that can handle these requirements?

 Is there an existing firmware protocol stack for something like this? I need to understand the firmware effort required.

 Thanks...

Brian

    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    Jan 26, 2022 1:49 PM UTC

    Hi @brian239955_stm1​ ,

    In STM32Cube firmware packages, there are the 2 following dedicated examples for sub-1GHz application:

    • STM32Cube_FW_L4\Projects\B-L475E-IOT01A\Applications\SubGhz
    • STM32Cube_FW_WL\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy

    This the software side, used hardware for each example is highlighted with blod characters.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.