Skip to main content
DBhut.1
Senior
Oct 7, 2022 9:55 AM UTC
Solved

Need an Ultra Low MCU which has RTC with 32-bit sub-second wakeup counter

Hello,

I am currently using STM32WLE5CC MCU, which has a great feature of RTC with 32-bit sub-second wakeup counter, But I need a low cost MCU for my other non lorawan project, which also need this "RTC with 32-bit sub-second wakeup counter" feature.

Please suggest MCU in Ultra low Power with RTC with 32-bit sub-second wakeup counter, and if this sub-second counter underflows, then it generates interrupt.

Thank You

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Oct 7, 2022 2:00 PM UTC

AN4759 has a nice table with RTC features across STM32 families.

However, what you are looking for is probably the binary mode, which is supported only by RTC v3 and also that only in 'WL and 'U5 families.

JW

5 replies

waclawek.jan
waclawek.janBest answer
Super User
Oct 7, 2022 2:00 PM UTC

AN4759 has a nice table with RTC features across STM32 families.

However, what you are looking for is probably the binary mode, which is supported only by RTC v3 and also that only in 'WL and 'U5 families.

JW

DBhut.1
DBhut.1Author
Senior
Oct 9, 2022 5:14 AM UTC

Thanks

Piranha
Principal III
Oct 19, 2022 8:30 PM UTC

Most likely he means RTC_WUTR register, which is present on most STM32 series. And that wake-up down-counter is 16-bit wide.

DBhut.1
DBhut.1Author
Senior
Oct 21, 2022 10:01 AM UTC

RTC_WUTR  doesn't have underflow interrupt.

Piranha
Principal III
Oct 23, 2022 8:54 PM UTC

Yeah, why would anyone read the reference manual...

"when it reaches 0, the WUTF flag is set in the RTC_SR register, and the wakeup counter is automatically reloaded with its reload value (RTC_WUTR register value)"

"When the periodic wakeup interrupt is enabled by setting the WUTIE bit in the RTC_CR register"